<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Problem with S32K148 and DP83848</title>
    <link>https://community.nxp.com/t5/S32K/Problem-with-S32K148-and-DP83848/m-p/1824976#M32765</link>
    <description>Hi&lt;BR /&gt;Thank you for your reply.I have checked Phy's initialization and found that the problem lies here.The problem has been solved now.&lt;BR /&gt;Regards</description>
    <pubDate>Mon, 11 Mar 2024 09:18:58 GMT</pubDate>
    <dc:creator>Zhangfeng1</dc:creator>
    <dc:date>2024-03-11T09:18:58Z</dc:date>
    <item>
      <title>Problem with S32K148 and DP83848</title>
      <link>https://community.nxp.com/t5/S32K/Problem-with-S32K148-and-DP83848/m-p/1818412#M32296</link>
      <description>&lt;P&gt;I am testing a controller board, whose main chip is S32K148 and network chip is DP83848. If I want to run the LWIP protocol stack, what parts do I need to modify on the official example? What other options may need to be modified besides modifying the MII option in the tcpip component when I use RMII for communication? The circuit of DP83848 has been verified on another controller and there is no problem.&lt;/P&gt;&lt;P&gt;Looking forward to your reply, thank you.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 06:52:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-with-S32K148-and-DP83848/m-p/1818412#M32296</guid>
      <dc:creator>Zhangfeng1</dc:creator>
      <dc:date>2024-02-29T06:52:04Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with S32K148 and DP83848</title>
      <link>https://community.nxp.com/t5/S32K/Problem-with-S32K148-and-DP83848/m-p/1821598#M32498</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;per my understanding no further setting would be needed. You can just check pin initialization if it corresponds to your connection.&lt;BR /&gt;No PHY init is done in demo, I think. PHY can be configured via strap options to run in some mode, and if it is the same with the option selected in tcpip component, no PHY init is required.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 05 Mar 2024 13:19:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-with-S32K148-and-DP83848/m-p/1821598#M32498</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-03-05T13:19:12Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with S32K148 and DP83848</title>
      <link>https://community.nxp.com/t5/S32K/Problem-with-S32K148-and-DP83848/m-p/1824976#M32765</link>
      <description>Hi&lt;BR /&gt;Thank you for your reply.I have checked Phy's initialization and found that the problem lies here.The problem has been solved now.&lt;BR /&gt;Regards</description>
      <pubDate>Mon, 11 Mar 2024 09:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-with-S32K148-and-DP83848/m-p/1824976#M32765</guid>
      <dc:creator>Zhangfeng1</dc:creator>
      <dc:date>2024-03-11T09:18:58Z</dc:date>
    </item>
  </channel>
</rss>