<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 FLEXRAM Usage As SRAM</title>
    <link>https://community.nxp.com/t5/S32K/FLEXRAM-Usage-As-SRAM/m-p/1824086#M32693</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to use FlexRam as SRAM in s32k116 microcontroller. In default, FlexRam is configured as RAM. How should I add FlexRam section to linker file?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to reduce SRAM usage which is 15kb in S32K116. That's why, I plan to use FlexRam as SRAM to add additional 2kb memory. I can not concatenate SRAM and FlexRam directly, because its start address is 0x1400 0000. I think that I probably need to define FlexRam in linker file and then I can store some data in FlexRam after defining it linker file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In order to store data in FlexRam, should I use "__attribute__"&amp;nbsp; ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 08 Mar 2024 10:19:53 GMT</pubDate>
    <dc:creator>kesanli_cinci</dc:creator>
    <dc:date>2024-03-08T10:19:53Z</dc:date>
    <item>
      <title>FLEXRAM Usage As SRAM</title>
      <link>https://community.nxp.com/t5/S32K/FLEXRAM-Usage-As-SRAM/m-p/1824086#M32693</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to use FlexRam as SRAM in s32k116 microcontroller. In default, FlexRam is configured as RAM. How should I add FlexRam section to linker file?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to reduce SRAM usage which is 15kb in S32K116. That's why, I plan to use FlexRam as SRAM to add additional 2kb memory. I can not concatenate SRAM and FlexRam directly, because its start address is 0x1400 0000. I think that I probably need to define FlexRam in linker file and then I can store some data in FlexRam after defining it linker file.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In order to store data in FlexRam, should I use "__attribute__"&amp;nbsp; ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Mar 2024 10:19:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLEXRAM-Usage-As-SRAM/m-p/1824086#M32693</guid>
      <dc:creator>kesanli_cinci</dc:creator>
      <dc:date>2024-03-08T10:19:53Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXRAM Usage As SRAM</title>
      <link>https://community.nxp.com/t5/S32K/FLEXRAM-Usage-As-SRAM/m-p/1824951#M32762</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229150"&gt;@kesanli_cinci&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;It was discussed in this thread:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/FLAXRAM-for-s32k144/m-p/1575503#M19702" target="_blank"&gt;https://community.nxp.com/t5/S32K/FLAXRAM-for-s32k144/m-p/1575503#M19702&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please have a look,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Mon, 11 Mar 2024 08:59:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FLEXRAM-Usage-As-SRAM/m-p/1824951#M32762</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-03-11T08:59:04Z</dc:date>
    </item>
  </channel>
</rss>