<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K144 FlexCAN Stop to Send Messages in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Stop-to-Send-Messages/m-p/832198#M3262</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;Please see Section 53.5.11.1 RM rev.8 Freeze mode.&lt;BR /&gt;“This mode is requested either by the CPU through the assertion of the HALT bit in the CAN_MCR Register or when the chip is put into Debug mode. In both cases it is also&amp;nbsp;necessary that the FRZ bit is asserted in the CAN_MCR Register and the module is not in a low-power mode.”&lt;/P&gt;&lt;P&gt;Freeze Enable is enabled by default MCR[FRZ] = 1. &lt;BR /&gt;And it will be disabled if you clear that bit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Oct 2018 19:48:51 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-10-08T19:48:51Z</dc:date>
    <item>
      <title>S32K144 FlexCAN Stop to Send Messages</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Stop-to-Send-Messages/m-p/832197#M3261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using S32K144 FlexCAN module. I met a problem now:&lt;/P&gt;&lt;P&gt;When I debug my source code, I set several break points. Every time when I start to run the SW after it stopped at a break point, then it will stop to send CAN messages. I want to know the root cause and how to avoid this case.&lt;/P&gt;&lt;P&gt;Thank you very much~~&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Oct 2018 02:06:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Stop-to-Send-Messages/m-p/832197#M3261</guid>
      <dc:creator>xiaoyuwang</dc:creator>
      <dc:date>2018-10-07T02:06:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 FlexCAN Stop to Send Messages</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Stop-to-Send-Messages/m-p/832198#M3262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;Please see Section 53.5.11.1 RM rev.8 Freeze mode.&lt;BR /&gt;“This mode is requested either by the CPU through the assertion of the HALT bit in the CAN_MCR Register or when the chip is put into Debug mode. In both cases it is also&amp;nbsp;necessary that the FRZ bit is asserted in the CAN_MCR Register and the module is not in a low-power mode.”&lt;/P&gt;&lt;P&gt;Freeze Enable is enabled by default MCR[FRZ] = 1. &lt;BR /&gt;And it will be disabled if you clear that bit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Oct 2018 19:48:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Stop-to-Send-Messages/m-p/832198#M3262</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-10-08T19:48:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 FlexCAN Stop to Send Messages</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Stop-to-Send-Messages/m-p/832199#M3263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi Daniel,&lt;/P&gt;&lt;P&gt;I have tried to enable Freeze Mode, it works.&amp;nbsp;&lt;/P&gt;&lt;P&gt;But I met another problem now: My ECU will receive 24 messages from vehicle and 3 messages for transmission. 2 messages are 20ms period(ID: 0x190, 0x191)，the third one is 500ms period(ID: 0x390). Sometimes when I start ECU, message 0x390 cannot be sent, but sometimes it is OK. Do you have any idea about this?&lt;/P&gt;&lt;P&gt;ps: Current BusLoad is 25.9%.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Oct 2018 05:56:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Stop-to-Send-Messages/m-p/832199#M3263</guid>
      <dc:creator>xiaoyuwang</dc:creator>
      <dc:date>2018-10-09T05:56:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 FlexCAN Stop to Send Messages</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Stop-to-Send-Messages/m-p/832200#M3264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Check for NOSTALL bit.&amp;nbsp;&lt;/P&gt;&lt;P&gt;make it high.&lt;/P&gt;&lt;P&gt;Hope it helps..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pritam.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Nov 2018 13:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Stop-to-Send-Messages/m-p/832200#M3264</guid>
      <dc:creator>pritampatil</dc:creator>
      <dc:date>2018-11-20T13:46:46Z</dc:date>
    </item>
  </channel>
</rss>