<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TRGMUX in S32K</title>
    <link>https://community.nxp.com/t5/S32K/TRGMUX/m-p/1822267#M32547</link>
    <description>1. is there another case?&lt;BR /&gt;2. do you have an example, how to so?</description>
    <pubDate>Wed, 06 Mar 2024 08:40:40 GMT</pubDate>
    <dc:creator>Ayaz</dc:creator>
    <dc:date>2024-03-06T08:40:40Z</dc:date>
    <item>
      <title>TRGMUX</title>
      <link>https://community.nxp.com/t5/S32K/TRGMUX/m-p/1821788#M32505</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I am trying to test the TRGMUX (input-output) functionality,&lt;/P&gt;&lt;P&gt;1) The output?&lt;/P&gt;&lt;P&gt;I am triggering&amp;nbsp; the emios_gpt every 25 us i have assigned the input into the TRGMUX as seen below:&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Skærmbillede 2024-03-05 182425.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266636i435D3DFC70D347EF/image-size/large?v=v2&amp;amp;px=999" role="button" title="Skærmbillede 2024-03-05 182425.png" alt="Skærmbillede 2024-03-05 182425.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;pin configurations: I have used the trgmux out1 -PTD-0&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Skærmbillede 2024-03-05 182637.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266637i5DFF74972759F06B/image-size/large?v=v2&amp;amp;px=999" role="button" title="Skærmbillede 2024-03-05 182637.png" alt="Skærmbillede 2024-03-05 182637.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I display the input signal from emios_gpt and the output signal from the TRGMUX&amp;nbsp; on the oscilloscope.&lt;/P&gt;&lt;P&gt;The issue I am seeing is that the emios_gpt signal frequency is 20 kHz and 50 duty cycle.&lt;/P&gt;&lt;P&gt;and the TRGMUX output signal is&amp;nbsp;40 kHz and 0,03 duty cycle.&lt;/P&gt;&lt;P&gt;The output frequency for the&amp;nbsp;TRGMUX is correct, but I was expecting to get the same signal the has been inputted. what do I miss here ??&lt;/P&gt;&lt;P&gt;2) input:&amp;nbsp; I would like to read a signal on a pin. How to configure the trgmux to read a signal from a pin?&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;I am using the s32k344 evaluation board&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Mar 2024 17:44:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TRGMUX/m-p/1821788#M32505</guid>
      <dc:creator>Ayaz</dc:creator>
      <dc:date>2024-03-05T17:44:10Z</dc:date>
    </item>
    <item>
      <title>Re: TRGMUX</title>
      <link>https://community.nxp.com/t5/S32K/TRGMUX/m-p/1822209#M32543</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Ayaz" target="_blank"&gt;Hi@Ayaz&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;First of all, I'm sorry, there are no more details about this part in the data sheet, so I don't have the ability to explain it clearly to you.&lt;/P&gt;
&lt;P&gt;However, I tested using-&amp;gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT size="2"&gt;&lt;STRONG&gt;TRGMUX_IP_INPUT_EMIOS0_RELOAD_OUT_CH0-&amp;gt;TRGMUX-&amp;gt;TRGMUX_IP_OUTPUT_BCTU_TRG23-&amp;gt;BCTU&lt;/STRONG&gt;,&lt;/FONT&gt; and the results were as expected.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_2-1709711359715.png" style="width: 565px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266740i2CF80786B443AB6A/image-dimensions/565x243?v=v2" width="565" height="243" role="button" title="Senlent_2-1709711359715.png" alt="Senlent_2-1709711359715.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_3-1709711391621.png" style="width: 563px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266741iAD75EC8EB0B89511/image-dimensions/563x470?v=v2" width="563" height="470" role="button" title="Senlent_3-1709711391621.png" alt="Senlent_3-1709711391621.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Here I suggest you use PWM-&amp;gt;TRGMUX-&amp;gt;BCTU to observe more details.&lt;BR /&gt;For example you can configure it like this:&lt;BR /&gt;&lt;STRONG&gt;&lt;FONT size="2"&gt;Chx_PWM-&amp;gt;TRGMUX_IP_INPUT_EMIOS0_IPP_CHx-&amp;gt;TRGMUX-&amp;gt;TRGMUX_IP_OUTPUT_BCTU_TRG23-&amp;gt;BCTU.&lt;/FONT&gt;&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&lt;FONT size="2"&gt;Chx_PWM-&amp;gt;TRGMUX_IP_INPUT_EMIOS0_IPP_CHx-&amp;gt;TRGMUX-&amp;gt;TRGMUX_IP_OUTPUT_SIUL2_0_3_OUTx&lt;/FONT&gt;&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Mar 2024 07:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TRGMUX/m-p/1822209#M32543</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-03-06T07:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: TRGMUX</title>
      <link>https://community.nxp.com/t5/S32K/TRGMUX/m-p/1822256#M32545</link>
      <description>Hi&lt;BR /&gt;Thanks for your response.&lt;BR /&gt;1 ) is there no explanation for this output behavior (the output signal duty cycle is been reduced, I was expecting to get the same input signal out without changes )?&lt;BR /&gt;2 ) is it possible to route an input signal from a physical pin as TRGMUX input ?&lt;BR /&gt;if yes , do you have an example project to refer to ?&lt;BR /&gt;BR&lt;BR /&gt;Ayaz&lt;BR /&gt;</description>
      <pubDate>Wed, 06 Mar 2024 08:34:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TRGMUX/m-p/1822256#M32545</guid>
      <dc:creator>Ayaz</dc:creator>
      <dc:date>2024-03-06T08:34:11Z</dc:date>
    </item>
    <item>
      <title>Re: TRGMUX</title>
      <link>https://community.nxp.com/t5/S32K/TRGMUX/m-p/1822262#M32546</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Ayaz" target="_blank"&gt;Hi@Ayaz&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;1. Yes, I did not find it, because few users use eMIOS_Gpt to trigger BCTU through TRGMUX&lt;/P&gt;
&lt;P&gt;2.I don't have such a routine, but this can be achieved, I think you just need to configure the correct input and output for TRGMUX, and then change the state of the input pin.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Mar 2024 08:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TRGMUX/m-p/1822262#M32546</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-03-06T08:38:24Z</dc:date>
    </item>
    <item>
      <title>Re: TRGMUX</title>
      <link>https://community.nxp.com/t5/S32K/TRGMUX/m-p/1822267#M32547</link>
      <description>1. is there another case?&lt;BR /&gt;2. do you have an example, how to so?</description>
      <pubDate>Wed, 06 Mar 2024 08:40:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TRGMUX/m-p/1822267#M32547</guid>
      <dc:creator>Ayaz</dc:creator>
      <dc:date>2024-03-06T08:40:40Z</dc:date>
    </item>
    <item>
      <title>Re: TRGMUX</title>
      <link>https://community.nxp.com/t5/S32K/TRGMUX/m-p/1822301#M32550</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Ayaz" target="_blank"&gt;Hi@Ayaz&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;“&amp;nbsp;is it possible to route an input signal from a physical pin as TRGMUX input”&lt;/P&gt;
&lt;P&gt;it should be easy to configure, for example:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1709715419281.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266758iCB8CA355485EDEA5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Senlent_0-1709715419281.png" alt="Senlent_0-1709715419281.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;then config pins for TRGMUX input and output.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Mar 2024 09:02:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/TRGMUX/m-p/1822301#M32550</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-03-06T09:02:33Z</dc:date>
    </item>
  </channel>
</rss>