<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックProgram a S32K from a 820A via SWD?</title>
    <link>https://community.nxp.com/t5/S32K/Program-a-S32K-from-a-820A-via-SWD/m-p/831378#M3251</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to setup an embedded system to be able to have a Snapdragon 820A program a S32K144 via SWD but it seems that 820A does not support SWD natively.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anybody would have seen a solution to do the above?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would there be a chip that can be the bridge between SPI and SWD for example?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could any GPIO be used on the 820A to become a SWD channel by creating custom timing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Dec 2018 23:52:04 GMT</pubDate>
    <dc:creator>perig_vennetier</dc:creator>
    <dc:date>2018-12-04T23:52:04Z</dc:date>
    <item>
      <title>Program a S32K from a 820A via SWD?</title>
      <link>https://community.nxp.com/t5/S32K/Program-a-S32K-from-a-820A-via-SWD/m-p/831378#M3251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'd like to setup an embedded system to be able to have a Snapdragon 820A program a S32K144 via SWD but it seems that 820A does not support SWD natively.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anybody would have seen a solution to do the above?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would there be a chip that can be the bridge between SPI and SWD for example?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could any GPIO be used on the 820A to become a SWD channel by creating custom timing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Dec 2018 23:52:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Program-a-S32K-from-a-820A-via-SWD/m-p/831378#M3251</guid>
      <dc:creator>perig_vennetier</dc:creator>
      <dc:date>2018-12-04T23:52:04Z</dc:date>
    </item>
  </channel>
</rss>