<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPD BIST_DIAGNOSTIC_CFG in S32K</title>
    <link>https://community.nxp.com/t5/S32K/SPD-BIST-DIAGNOSTIC-CFG/m-p/1820758#M32444</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;If you don't have a timing requirement it's possible to run the BIST_DIAGNOSTIC_CFG. Just consider that the BIST_SAFETYBOOT_CFG has enough coverage with almost 10 ms saved&lt;/P&gt;</description>
    <pubDate>Mon, 04 Mar 2024 17:29:49 GMT</pubDate>
    <dc:creator>martinkaspar-r3</dc:creator>
    <dc:date>2024-03-04T17:29:49Z</dc:date>
    <item>
      <title>SPD BIST_DIAGNOSTIC_CFG</title>
      <link>https://community.nxp.com/t5/S32K/SPD-BIST-DIAGNOSTIC-CFG/m-p/1818835#M32332</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;is it possible to run Bist_Run( BIST_DIAGNOSTIC_CFG ) at boot and not&amp;nbsp;BIST_SAFETYBOOT_CFG ?&lt;/P&gt;&lt;P&gt;In our application there is no poweron timing costraints, so the 10ms execution time of the full featured Bist&amp;nbsp; "BIST_DIAGNOSTIC_CFG" is not a problem.&lt;/P&gt;&lt;P&gt;Also, off chip FS26 doesn't reset the onboard and at boot time there are all the "garage" conditions required.&lt;/P&gt;&lt;P&gt;Finally in pre defined "parking"(for example) conditions we reset ECU in order to perform&amp;nbsp;BIST_DIAGNOSTIC_CFG.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Fabio&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 14:22:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPD-BIST-DIAGNOSTIC-CFG/m-p/1818835#M32332</guid>
      <dc:creator>FabioG</dc:creator>
      <dc:date>2024-02-29T14:22:27Z</dc:date>
    </item>
    <item>
      <title>Re: SPD BIST_DIAGNOSTIC_CFG</title>
      <link>https://community.nxp.com/t5/S32K/SPD-BIST-DIAGNOSTIC-CFG/m-p/1820758#M32444</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;If you don't have a timing requirement it's possible to run the BIST_DIAGNOSTIC_CFG. Just consider that the BIST_SAFETYBOOT_CFG has enough coverage with almost 10 ms saved&lt;/P&gt;</description>
      <pubDate>Mon, 04 Mar 2024 17:29:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPD-BIST-DIAGNOSTIC-CFG/m-p/1820758#M32444</guid>
      <dc:creator>martinkaspar-r3</dc:creator>
      <dc:date>2024-03-04T17:29:49Z</dc:date>
    </item>
  </channel>
</rss>