<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックControlling LED intensity</title>
    <link>https://community.nxp.com/t5/S32K/Controlling-LED-intensity/m-p/1820563#M32432</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to use pwm signle (OPWMB mode) to control a blue, red, and green LED color at a frequency of 1.5Hz via emios_pwm.&lt;BR /&gt;Without adjusting the global prescaler, how can I scale the emios_mcl to produce 1.5 Hz?&lt;BR /&gt;What options are there?&lt;BR /&gt;What is the lowest emios_mcl frequency that we can achieve both with and without modifying the global prescaler's value?&lt;/P&gt;</description>
    <pubDate>Mon, 04 Mar 2024 13:10:57 GMT</pubDate>
    <dc:creator>Ayaz</dc:creator>
    <dc:date>2024-03-04T13:10:57Z</dc:date>
    <item>
      <title>Controlling LED intensity</title>
      <link>https://community.nxp.com/t5/S32K/Controlling-LED-intensity/m-p/1820563#M32432</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to use pwm signle (OPWMB mode) to control a blue, red, and green LED color at a frequency of 1.5Hz via emios_pwm.&lt;BR /&gt;Without adjusting the global prescaler, how can I scale the emios_mcl to produce 1.5 Hz?&lt;BR /&gt;What options are there?&lt;BR /&gt;What is the lowest emios_mcl frequency that we can achieve both with and without modifying the global prescaler's value?&lt;/P&gt;</description>
      <pubDate>Mon, 04 Mar 2024 13:10:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Controlling-LED-intensity/m-p/1820563#M32432</guid>
      <dc:creator>Ayaz</dc:creator>
      <dc:date>2024-03-04T13:10:57Z</dc:date>
    </item>
    <item>
      <title>Re: Controlling LED intensity</title>
      <link>https://community.nxp.com/t5/S32K/Controlling-LED-intensity/m-p/1821280#M32473</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Ayaz" target="_blank"&gt;Hi@Ayaz&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;For example, the eMIOSn_Chx's clock source is 48MHz and with default prescaler(1).&lt;/P&gt;
&lt;P&gt;The timer width is 16 bits which means the max counter value is 65535.&lt;/P&gt;
&lt;P&gt;The the lowest frequency is 48MHz / (65535 * 1S) ≈ 732.433Hz.&lt;/P&gt;</description>
      <pubDate>Tue, 05 Mar 2024 08:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Controlling-LED-intensity/m-p/1821280#M32473</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-03-05T08:16:01Z</dc:date>
    </item>
  </channel>
</rss>