<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Unified Bootloader Binaries</title>
    <link>https://community.nxp.com/t5/S32K/Unified-Bootloader-Binaries/m-p/1820131#M32393</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188029"&gt;@Senlent&lt;/a&gt;&lt;/P&gt;&lt;P&gt;Thanks for the speedy reply! When I tried compiling the flash bin file, I got an error saying Mca1.h and C40_Ip.h was not found. Moreover, my linker files looked very different compared to the image. Should I create the project as a new S32K application or am I missing any steps during project creation?&lt;/P&gt;&lt;P&gt;I'll try again in the morning following the article.&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Grasshopper&lt;/P&gt;</description>
    <pubDate>Mon, 04 Mar 2024 05:27:03 GMT</pubDate>
    <dc:creator>Grasshopper1</dc:creator>
    <dc:date>2024-03-04T05:27:03Z</dc:date>
    <item>
      <title>Unified Bootloader Binaries</title>
      <link>https://community.nxp.com/t5/S32K/Unified-Bootloader-Binaries/m-p/1819972#M32383</link>
      <description>&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;I'm using&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099" target="_self"&gt;the Unified UDS Bootloader for S32K boards&lt;/A&gt;&amp;nbsp;as a baseline for my project. So far, I have gotten both the desktop application and the firmware running, and I have been able to send an update and flash the board using the desktop application.&lt;/P&gt;&lt;P&gt;However, I do not understand how the binaries "flash_api.bin" and "S32k144_CANFD.bin" are generated. I assumed the latter is simply the compiled version of the provided source code, but the .bin file I generated through compiling the source code is larger, and temporarily disables the board until another project is flashed.&lt;/P&gt;&lt;P&gt;I have also followed the description given by&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188029"&gt;@Senlent&lt;/a&gt;&amp;nbsp;as a comment in the project post; however, I am still very confused about how to compile the "flash_api.bin". Can I have the source code for it and a description to how I can compile sources to be flashed using the app?&lt;/P&gt;&lt;P&gt;Any replies are greatly appreciated!&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Grasshopper&lt;/P&gt;</description>
      <pubDate>Sun, 03 Mar 2024 19:59:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unified-Bootloader-Binaries/m-p/1819972#M32383</guid>
      <dc:creator>Grasshopper1</dc:creator>
      <dc:date>2024-03-03T19:59:02Z</dc:date>
    </item>
    <item>
      <title>Re: Unified Bootloader Binaries</title>
      <link>https://community.nxp.com/t5/S32K/Unified-Bootloader-Binaries/m-p/1820034#M32387</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Grasshopper1" target="_blank"&gt;Hi@Grasshopper1&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;1.This is an article I wrote before to explain what flash bin is.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K-How-to-make-Flash-Driver-image/ta-p/1630873" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K-How-to-make-Flash-Driver-image/ta-p/1630873&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;2.I have clearly written how to create a flash bin file in the comment on the link you provided, and the source file is also in this comment.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1709519394847.png" style="width: 469px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266148i4D60CF03F56CCB8F/image-dimensions/469x355?v=v2" width="469" height="355" role="button" title="Senlent_0-1709519394847.png" alt="Senlent_0-1709519394847.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Senlent_0-1709519394847.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Mar 2024 02:31:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unified-Bootloader-Binaries/m-p/1820034#M32387</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-03-04T02:31:04Z</dc:date>
    </item>
    <item>
      <title>Re: Unified Bootloader Binaries</title>
      <link>https://community.nxp.com/t5/S32K/Unified-Bootloader-Binaries/m-p/1820131#M32393</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/188029"&gt;@Senlent&lt;/a&gt;&lt;/P&gt;&lt;P&gt;Thanks for the speedy reply! When I tried compiling the flash bin file, I got an error saying Mca1.h and C40_Ip.h was not found. Moreover, my linker files looked very different compared to the image. Should I create the project as a new S32K application or am I missing any steps during project creation?&lt;/P&gt;&lt;P&gt;I'll try again in the morning following the article.&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Grasshopper&lt;/P&gt;</description>
      <pubDate>Mon, 04 Mar 2024 05:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Unified-Bootloader-Binaries/m-p/1820131#M32393</guid>
      <dc:creator>Grasshopper1</dc:creator>
      <dc:date>2024-03-04T05:27:03Z</dc:date>
    </item>
  </channel>
</rss>