<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32K312 MCAL WDG Not Working in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-MCAL-WDG-Not-Working/m-p/1818392#M32294</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to implement a Watchdog for S32K312 through MCAL's WDG module. I am using the MCAL version of R21-11_4.0.0_P01_D2312.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have set up the GPT timer,WDG module WIT is set to 3.5 seconds, WTP is set to 1 second, WWP is set to 0.05 seconds.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The program calls Wdg_ChannelInit( WDG_IPW_INSTANCE0,NULL_PTR ) and WdgIf_SetMode(WDG_IPW_INSTANCE0,WDGIF_SLOW_MODE),&lt;BR /&gt;and calls WdgIf_SetTriggerCondition(WDG_IPW_INSTANCE0,2500) every 500mS.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;But the program executes Reset when it reaches Swt_Ip_ServiceCmd(Base, SWT_IP_FIXED_SERVICE_VALUE1_U16), and the WDG time is not cleared. What am I doing wrong?&lt;/P&gt;</description>
    <pubDate>Thu, 29 Feb 2024 06:16:08 GMT</pubDate>
    <dc:creator>Jacky_00001</dc:creator>
    <dc:date>2024-02-29T06:16:08Z</dc:date>
    <item>
      <title>S32K312 MCAL WDG Not Working</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-MCAL-WDG-Not-Working/m-p/1818392#M32294</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to implement a Watchdog for S32K312 through MCAL's WDG module. I am using the MCAL version of R21-11_4.0.0_P01_D2312.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I have set up the GPT timer,WDG module WIT is set to 3.5 seconds, WTP is set to 1 second, WWP is set to 0.05 seconds.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The program calls Wdg_ChannelInit( WDG_IPW_INSTANCE0,NULL_PTR ) and WdgIf_SetMode(WDG_IPW_INSTANCE0,WDGIF_SLOW_MODE),&lt;BR /&gt;and calls WdgIf_SetTriggerCondition(WDG_IPW_INSTANCE0,2500) every 500mS.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;But the program executes Reset when it reaches Swt_Ip_ServiceCmd(Base, SWT_IP_FIXED_SERVICE_VALUE1_U16), and the WDG time is not cleared. What am I doing wrong?&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 06:16:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-MCAL-WDG-Not-Working/m-p/1818392#M32294</guid>
      <dc:creator>Jacky_00001</dc:creator>
      <dc:date>2024-02-29T06:16:08Z</dc:date>
    </item>
  </channel>
</rss>