<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CAN BUS in S32K</title>
    <link>https://community.nxp.com/t5/S32K/CAN-BUS/m-p/1818385#M32292</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;no, you have no such info about faulty message.&amp;nbsp;&lt;SPAN&gt;Module does not store received CRC and moreover if error is detected a message is not moved-in into given MB. Just error free messages are stored, but without CRC info.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Feb 2024 06:03:43 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2024-02-29T06:03:43Z</dc:date>
    <item>
      <title>CAN BUS</title>
      <link>https://community.nxp.com/t5/S32K/CAN-BUS/m-p/1814946#M32057</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wutengyouxi555_0-1708768900958.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/264855i1B8A7BF0E3A2E1DB/image-size/medium?v=v2&amp;amp;px=400" alt="wutengyouxi555_0-1708768900958.png" title="wutengyouxi555_0-1708768900958.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This function is canerr callback function from s32k144 SDK 4.0.2&amp;nbsp;&lt;/P&gt;&lt;P&gt;How CAN I know what kind of err has happened on the CAN bus from this Function.&lt;/P&gt;</description>
      <pubDate>Sat, 24 Feb 2024 10:05:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-BUS/m-p/1814946#M32057</guid>
      <dc:creator>wutengyouxi555</dc:creator>
      <dc:date>2024-02-24T10:05:20Z</dc:date>
    </item>
    <item>
      <title>Re: CAN BUS</title>
      <link>https://community.nxp.com/t5/S32K/CAN-BUS/m-p/1815628#M32123</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;calling&amp;nbsp;FLEXCAN_DRV_GetErrorStatus (reading ESR1) you clears status error bits. So read it into some status variable and mask/check as needed. You can refer to&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-FlexCAN-TX-RX-Error-ISR-test-S32DS2-2/ta-p/1278224" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-FlexCAN-TX-RX-Error-ISR-test-S32DS2-2/ta-p/1278224&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Feb 2024 13:34:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-BUS/m-p/1815628#M32123</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-02-26T13:34:27Z</dc:date>
    </item>
    <item>
      <title>Re: CAN BUS</title>
      <link>https://community.nxp.com/t5/S32K/CAN-BUS/m-p/1817346#M32242</link>
      <description>Thinks your help. One more question，if a CRC err occurs , could i know which message is this error coming from ?</description>
      <pubDate>Wed, 28 Feb 2024 09:23:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-BUS/m-p/1817346#M32242</guid>
      <dc:creator>wutengyouxi555</dc:creator>
      <dc:date>2024-02-28T09:23:02Z</dc:date>
    </item>
    <item>
      <title>Re: CAN BUS</title>
      <link>https://community.nxp.com/t5/S32K/CAN-BUS/m-p/1818385#M32292</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;no, you have no such info about faulty message.&amp;nbsp;&lt;SPAN&gt;Module does not store received CRC and moreover if error is detected a message is not moved-in into given MB. Just error free messages are stored, but without CRC info.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 06:03:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-BUS/m-p/1818385#M32292</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-02-29T06:03:43Z</dc:date>
    </item>
  </channel>
</rss>