<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックEmios(PWM-GPT)</title>
    <link>https://community.nxp.com/t5/S32K/Emios-PWM-GPT/m-p/1817728#M32269</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;To provide the period to Emios_pwm, I use the Emios_mcl driver. In addition, I use Emios_gpt to trigger the BCTU.&lt;/P&gt;&lt;P&gt;My issue is that&amp;nbsp;when the emios_gpt is activated. emios_pwm outputs a default value ??,&amp;nbsp; What may be the cause of this ?&lt;/P&gt;&lt;P&gt;I am using S32K344 evolution board.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Ayaz&lt;/P&gt;</description>
    <pubDate>Wed, 28 Feb 2024 18:01:36 GMT</pubDate>
    <dc:creator>Ayaz</dc:creator>
    <dc:date>2024-02-28T18:01:36Z</dc:date>
    <item>
      <title>Emios(PWM-GPT)</title>
      <link>https://community.nxp.com/t5/S32K/Emios-PWM-GPT/m-p/1817728#M32269</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;To provide the period to Emios_pwm, I use the Emios_mcl driver. In addition, I use Emios_gpt to trigger the BCTU.&lt;/P&gt;&lt;P&gt;My issue is that&amp;nbsp;when the emios_gpt is activated. emios_pwm outputs a default value ??,&amp;nbsp; What may be the cause of this ?&lt;/P&gt;&lt;P&gt;I am using S32K344 evolution board.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Ayaz&lt;/P&gt;</description>
      <pubDate>Wed, 28 Feb 2024 18:01:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Emios-PWM-GPT/m-p/1817728#M32269</guid>
      <dc:creator>Ayaz</dc:creator>
      <dc:date>2024-02-28T18:01:36Z</dc:date>
    </item>
    <item>
      <title>Re: Emios(PWM-GPT)</title>
      <link>https://community.nxp.com/t5/S32K/Emios-PWM-GPT/m-p/1818460#M32299</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Ayaz" target="_blank"&gt;Hi@Ayaz&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;I can't see how EMIOS triggers Bctu when used as Gpt, but I guess it is based on some flags or internal outputs&lt;/P&gt;
&lt;P&gt;"To request an ADC conversion through the BCTU, a timer module such as eMIOS asserts its output signal, which is connected to a BCTU trigger input."&lt;/P&gt;
&lt;P&gt;I hope you can read the data sheet later or write some test code yourself. This is the test routine I made for Gpt-&amp;gt;Bctu-&amp;gt;Adc. You can refer to it.&lt;/P&gt;
&lt;P&gt;Trigger sequence&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1709191936556.png" style="width: 541px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/265736i0929F27AFEDBEBDF/image-dimensions/541x170?v=v2" width="541" height="170" role="button" title="Senlent_0-1709191936556.png" alt="Senlent_0-1709191936556.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Adc result&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_1-1709191952153.png" style="width: 555px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/265737i844499E9DC247AF2/image-dimensions/555x111?v=v2" width="555" height="111" role="button" title="Senlent_1-1709191952153.png" alt="Senlent_1-1709191952153.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 07:47:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Emios-PWM-GPT/m-p/1818460#M32299</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-02-29T07:47:29Z</dc:date>
    </item>
  </channel>
</rss>