<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IPCF of S32K3 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/IPCF-of-S32K3/m-p/1816448#M32159</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi All,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I c&lt;SPAN&gt;reate&amp;nbsp;&lt;/SPAN&gt;a S32DS Application Project of s32k324, and want to use IPCF.&lt;/P&gt;&lt;P&gt;I have INSTALLED the follow items as sequence&lt;/P&gt;&lt;P&gt;1. S32DS_3.4&lt;BR /&gt;2. S32 Design Studio IDE 3.4 Update 3&lt;BR /&gt;3. SW32K3_RTD_4_4_2_0_0_D2203&lt;BR /&gt;4. FreeRTOS v10.4.6_2.0.0_D2204&lt;BR /&gt;5. NXP GCC 10.2.0 20200723&lt;BR /&gt;6. SW32K3_IPCF_3.6.0_D2206&lt;/P&gt;&lt;P&gt;But&amp;nbsp; I can not add ipcf at&amp;nbsp;Graphical programming interface.&lt;/P&gt;&lt;P&gt;If I&amp;nbsp;c&lt;SPAN&gt;reate&amp;nbsp;S32DS Project from Example,there is ipcf middleware.The example can build correctly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What conditions affect peripheral components in graphical programming interfaces?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 27 Feb 2024 09:37:10 GMT</pubDate>
    <dc:creator>FrankLiu2019</dc:creator>
    <dc:date>2024-02-27T09:37:10Z</dc:date>
    <item>
      <title>IPCF of S32K3</title>
      <link>https://community.nxp.com/t5/S32K/IPCF-of-S32K3/m-p/1816448#M32159</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi All,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I c&lt;SPAN&gt;reate&amp;nbsp;&lt;/SPAN&gt;a S32DS Application Project of s32k324, and want to use IPCF.&lt;/P&gt;&lt;P&gt;I have INSTALLED the follow items as sequence&lt;/P&gt;&lt;P&gt;1. S32DS_3.4&lt;BR /&gt;2. S32 Design Studio IDE 3.4 Update 3&lt;BR /&gt;3. SW32K3_RTD_4_4_2_0_0_D2203&lt;BR /&gt;4. FreeRTOS v10.4.6_2.0.0_D2204&lt;BR /&gt;5. NXP GCC 10.2.0 20200723&lt;BR /&gt;6. SW32K3_IPCF_3.6.0_D2206&lt;/P&gt;&lt;P&gt;But&amp;nbsp; I can not add ipcf at&amp;nbsp;Graphical programming interface.&lt;/P&gt;&lt;P&gt;If I&amp;nbsp;c&lt;SPAN&gt;reate&amp;nbsp;S32DS Project from Example,there is ipcf middleware.The example can build correctly.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What conditions affect peripheral components in graphical programming interfaces?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Feb 2024 09:37:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/IPCF-of-S32K3/m-p/1816448#M32159</guid>
      <dc:creator>FrankLiu2019</dc:creator>
      <dc:date>2024-02-27T09:37:10Z</dc:date>
    </item>
    <item>
      <title>Re: IPCF of S32K3</title>
      <link>https://community.nxp.com/t5/S32K/IPCF-of-S32K3/m-p/1817242#M32225</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I have INSTALLED the follow items as sequence&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;1.S32DS_3.5&lt;/P&gt;&lt;P&gt;2.SW32K39x_S32DS_3.5.6_D2309&lt;/P&gt;&lt;P&gt;3.SW32K3_RTD_4.4_R21-11_3.0.0_D2303_DS_updatesite&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;4.SW32K3_FreeRTOS_10_5_1_UOS_3_1_0_DS_updatesite_D2304&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;5.SW32K3_IPCF_4.0.0_D2306_updatesite&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Then the problem was solved.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Feb 2024 08:04:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/IPCF-of-S32K3/m-p/1817242#M32225</guid>
      <dc:creator>FrankLiu2019</dc:creator>
      <dc:date>2024-02-28T08:04:18Z</dc:date>
    </item>
  </channel>
</rss>