<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックHow can I let the CAN enter Stop Mode</title>
    <link>https://community.nxp.com/t5/S32K/How-can-I-let-the-CAN-enter-Stop-Mode/m-p/826366#M3193</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;as the S32Kxx-RM description,the CAN enter the Stop mode,the first step is enter Freeze mode ,and then Stop mode is requested at chip level.&lt;/P&gt;&lt;P&gt;Is there the "chip level Stop" mean "CPU Stop"?If yes,then cpu stop ,how I can know whether the CAN had enter Stop mode?&lt;/P&gt;&lt;P&gt;&amp;nbsp;Is there have a exmple for CAN stop and wakeup? thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Nov 2018 02:53:10 GMT</pubDate>
    <dc:creator>春华张</dc:creator>
    <dc:date>2018-11-12T02:53:10Z</dc:date>
    <item>
      <title>How can I let the CAN enter Stop Mode</title>
      <link>https://community.nxp.com/t5/S32K/How-can-I-let-the-CAN-enter-Stop-Mode/m-p/826366#M3193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;as the S32Kxx-RM description,the CAN enter the Stop mode,the first step is enter Freeze mode ,and then Stop mode is requested at chip level.&lt;/P&gt;&lt;P&gt;Is there the "chip level Stop" mean "CPU Stop"?If yes,then cpu stop ,how I can know whether the CAN had enter Stop mode?&lt;/P&gt;&lt;P&gt;&amp;nbsp;Is there have a exmple for CAN stop and wakeup? thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Nov 2018 02:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-can-I-let-the-CAN-enter-Stop-Mode/m-p/826366#M3193</guid>
      <dc:creator>春华张</dc:creator>
      <dc:date>2018-11-12T02:53:10Z</dc:date>
    </item>
    <item>
      <title>Re: How can I let the CAN enter Stop Mode</title>
      <link>https://community.nxp.com/t5/S32K/How-can-I-let-the-CAN-enter-Stop-Mode/m-p/826367#M3194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;Yes, the chip level stop is entered once WFI instruction is executed.&lt;BR /&gt;“If FlexCAN receives the global Stop mode request during Freeze mode, it sets the LPMACK bit, negates the FRZACK bit and then sends the Stop Acknowledge signal to&amp;nbsp;the CPU, in order to shut down the clocks globally.” (Section 53.5.11.3 RM rev.9).&amp;nbsp;Please see Section 25.2.2.6 Stop mode acknowledge error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2018 21:04:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/How-can-I-let-the-CAN-enter-Stop-Mode/m-p/826367#M3194</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-11-21T21:04:17Z</dc:date>
    </item>
  </channel>
</rss>