<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックBalancing blocks MC3371C</title>
    <link>https://community.nxp.com/t5/S32K/Balancing-blocks-MC3371C/m-p/1810678#M31792</link>
    <description>&lt;P&gt;Hi everyone!&lt;/P&gt;&lt;P&gt;I have a doubt or problem of balancing.&lt;/P&gt;&lt;P&gt;I am seeing the datasheet of BMS and I can check that the current for the passive balancing process is 300 mA. I have the resistors set in the evaluation PCB correctly but only I obtained 200 mA of current maxim.&lt;BR /&gt;&lt;BR /&gt;Could you tell me if it could reach 300 mA somehow? Would the CHIP actually support 300 mA?&lt;BR /&gt;&lt;BR /&gt;I am currently balancing in order, i.e. if cells 1, 5, and 7 are unbalanced, it starts balancing in order (1 to 7) regardless of the voltage level of each cell.&amp;nbsp;But what would be the correct priority based on voltage?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;To improve the balancing sequence, it is being taken into account that contiguous cells should not be balanced.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;</description>
    <pubDate>Mon, 19 Feb 2024 08:03:25 GMT</pubDate>
    <dc:creator>sylvya_8214</dc:creator>
    <dc:date>2024-02-19T08:03:25Z</dc:date>
    <item>
      <title>Balancing blocks MC3371C</title>
      <link>https://community.nxp.com/t5/S32K/Balancing-blocks-MC3371C/m-p/1810678#M31792</link>
      <description>&lt;P&gt;Hi everyone!&lt;/P&gt;&lt;P&gt;I have a doubt or problem of balancing.&lt;/P&gt;&lt;P&gt;I am seeing the datasheet of BMS and I can check that the current for the passive balancing process is 300 mA. I have the resistors set in the evaluation PCB correctly but only I obtained 200 mA of current maxim.&lt;BR /&gt;&lt;BR /&gt;Could you tell me if it could reach 300 mA somehow? Would the CHIP actually support 300 mA?&lt;BR /&gt;&lt;BR /&gt;I am currently balancing in order, i.e. if cells 1, 5, and 7 are unbalanced, it starts balancing in order (1 to 7) regardless of the voltage level of each cell.&amp;nbsp;But what would be the correct priority based on voltage?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;To improve the balancing sequence, it is being taken into account that contiguous cells should not be balanced.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;</description>
      <pubDate>Mon, 19 Feb 2024 08:03:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Balancing-blocks-MC3371C/m-p/1810678#M31792</guid>
      <dc:creator>sylvya_8214</dc:creator>
      <dc:date>2024-02-19T08:03:25Z</dc:date>
    </item>
    <item>
      <title>Re: Balancing blocks MC3371C</title>
      <link>https://community.nxp.com/t5/S32K/Balancing-blocks-MC3371C/m-p/1811521#M31834</link>
      <description>&lt;P&gt;You can refer to below for this CB function--VCELL/(RBAL + RBAL_C + 0.5 Ω)&lt;BR /&gt;calculates the maximum cell balancing current, which is up to 300 mA:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="guoweisun_0-1708411501490.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/263917iDE46CA8C435F1D34/image-size/medium?v=v2&amp;amp;px=400" role="button" title="guoweisun_0-1708411501490.png" alt="guoweisun_0-1708411501490.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;guoweisun_0-1708411501490.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Feb 2024 06:45:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Balancing-blocks-MC3371C/m-p/1811521#M31834</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2024-02-20T06:45:43Z</dc:date>
    </item>
  </channel>
</rss>