<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problem is power supply to the S32K3X4-T172 board in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1809019#M31718</link>
    <description>&lt;P&gt;I tried to watch voltage level from different jumpers and trackpoints.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;P3V3 and&amp;nbsp;+3.3 Volts Power Supply is working fine.&lt;BR /&gt;&lt;BR /&gt;The&amp;nbsp;P5V0 is 0 V, I measured it from TP26 and J39.13. This is when jumpers are in default position.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;But when I make the J18 jumper open, all D1, D2, D4, D5 LEDs starts glowing and the TP26 shows 5 V in the oscilloscope.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Can you suggest me the solution from above information ? Please let me know if you need any more information.&lt;BR /&gt;&lt;BR /&gt;Attached Image shows LEDs when jumper 18 is in OPEN position.&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 15 Feb 2024 10:17:47 GMT</pubDate>
    <dc:creator>SParihar</dc:creator>
    <dc:date>2024-02-15T10:17:47Z</dc:date>
    <item>
      <title>Problem is power supply to the S32K3X4-T172 board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1804663#M31574</link>
      <description>&lt;P&gt;I am proving 12V 2 A power to the board, but only D2 LED glows. D4 and D5 LED remain OFF even when I turn ON the switch. Are there any solution for this problem.&lt;BR /&gt;The board was working correctly few days ago.&lt;/P&gt;</description>
      <pubDate>Fri, 09 Feb 2024 12:28:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1804663#M31574</guid>
      <dc:creator>SParihar</dc:creator>
      <dc:date>2024-02-09T12:28:24Z</dc:date>
    </item>
    <item>
      <title>Re: Problem is power supply to the S32K3X4-T172 board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1804893#M31578</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220636"&gt;@SParihar&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;D2 LED &lt;SPAN&gt;show the presence of the supply voltage (12V) from the adaptor. Please help me confirming the jumper configurations from the&amp;nbsp;&lt;A href="https://www.nxp.com/document/guide/getting-started-with-the-s32k3x4evb-t172-evaluation-board-for-automotive-general-purpose:GS-S32K3X4EVB-T172?section=plug-it-in" target="_blank"&gt;Getting Started with the S32K3X4EVB-T172&lt;/A&gt;&amp;nbsp;guide, as well as the switch position and the debugger cable.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please update me on any findings.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;BR /&gt;Julián.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Feb 2024 19:16:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1804893#M31578</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-02-09T19:16:30Z</dc:date>
    </item>
    <item>
      <title>Re: Problem is power supply to the S32K3X4-T172 board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1804988#M31582</link>
      <description>All jumpers are on default position. I am using a micro usb SDA cable for debugging. I am following the hardware manual when turning ON the board, switching power switch SW1 from position 2-3 to 1-2 when adapter is connected.&lt;BR /&gt;It was working correctly few days ago.</description>
      <pubDate>Sat, 10 Feb 2024 05:24:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1804988#M31582</guid>
      <dc:creator>SParihar</dc:creator>
      <dc:date>2024-02-10T05:24:24Z</dc:date>
    </item>
    <item>
      <title>Re: Problem is power supply to the S32K3X4-T172 board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1805339#M31604</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220636"&gt;@SParihar&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please help me checking the voltage source for the board, as if no LEDs are illuminated when power is applied to the EVB and the regulators are correctly enabled using the appropriate jumpers, it is possible that either power supply is not connected properly, or the voltage level is lower that the specified [&lt;STRONG&gt;+12.0V&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;to ≥2Amps&lt;/STRONG&gt;].&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;Note that the fuse will not protect against one of the EVB regulators being shorted. If this happens, damage is likely to occur to the EVB and/or components.&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Mon, 12 Feb 2024 15:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1805339#M31604</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-02-12T15:51:59Z</dc:date>
    </item>
    <item>
      <title>Re: Problem is power supply to the S32K3X4-T172 board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1806300#M31654</link>
      <description>D2 LED turns ON, means supply voltage is correct. The problem is in the board, maybe it has been damaged because D4 and D5 LED are not glowing.</description>
      <pubDate>Wed, 14 Feb 2024 06:10:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1806300#M31654</guid>
      <dc:creator>SParihar</dc:creator>
      <dc:date>2024-02-14T06:10:07Z</dc:date>
    </item>
    <item>
      <title>Re: Problem is power supply to the S32K3X4-T172 board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1808762#M31685</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220636"&gt;@SParihar&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you help me measuring the voltage levels on the MCU? You can follow these guidelines:&amp;nbsp;&lt;A href="https://www.nxp.jp/docs/en/application-note/AN13461.pdf" target="_blank"&gt;AN13461: NXP Microcontroller Troubleshooting Checklist - Application Note&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;A component in your board could be faulty and causing no voltage to be powered into the MCU.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Feb 2024 22:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1808762#M31685</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-02-14T22:49:51Z</dc:date>
    </item>
    <item>
      <title>Re: Problem is power supply to the S32K3X4-T172 board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1809019#M31718</link>
      <description>&lt;P&gt;I tried to watch voltage level from different jumpers and trackpoints.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;P3V3 and&amp;nbsp;+3.3 Volts Power Supply is working fine.&lt;BR /&gt;&lt;BR /&gt;The&amp;nbsp;P5V0 is 0 V, I measured it from TP26 and J39.13. This is when jumpers are in default position.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;But when I make the J18 jumper open, all D1, D2, D4, D5 LEDs starts glowing and the TP26 shows 5 V in the oscilloscope.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Can you suggest me the solution from above information ? Please let me know if you need any more information.&lt;BR /&gt;&lt;BR /&gt;Attached Image shows LEDs when jumper 18 is in OPEN position.&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 15 Feb 2024 10:17:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1809019#M31718</guid>
      <dc:creator>SParihar</dc:creator>
      <dc:date>2024-02-15T10:17:47Z</dc:date>
    </item>
    <item>
      <title>Re: Problem is power supply to the S32K3X4-T172 board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1809569#M31736</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220636"&gt;@SParihar&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you confirm the voltage supply in FS26 when J18 is in 2-3 position? This should return the 3.3v value. By removing J18, no voltage should be active&amp;nbsp;&lt;SPAN&gt;for the VDD_HV_A domain, as stated in the Hardware User Manual:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1708035263932.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/263387iBD64B15351207462/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1708035263932.png" alt="Julin_AragnM_0-1708035263932.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Also, please help me going into the Hardware Design resources, and confirming the voltage connections&amp;nbsp;for LDO1OUT1/2, in case of any burned components before the&amp;nbsp;FS26ZZXMA0D.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_1-1708036082346.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/263388iA17E1AB5FA2964C2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_1-1708036082346.png" alt="Julin_AragnM_1-1708036082346.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Feb 2024 22:30:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1809569#M31736</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-02-15T22:30:11Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in power supply to the S32K3X4-T172 board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1809751#M31740</link>
      <description>&lt;P&gt;When connecting the J18 in 2-3 position, J427 gives nearly 0V. Which is similar to what was happening when J18 was in 1-2 position, J427 was 0V.&lt;/P&gt;&lt;P&gt;But when I open the J427,&amp;nbsp;&lt;BR /&gt;1. VDD_HV_A = 5V for position 1-2 in J18;&lt;BR /&gt;2. VDD_HV_A = 3.3 V for posotion 2-3 in J18 (voltage measured from pin 2 of J427).&lt;BR /&gt;3. D3 RED LED of RESET_K3 starts glowing for positions 1-2 and 2-3 of J18.&lt;BR /&gt;&lt;BR /&gt;I think the problem is due to the pin 1 of J427.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;I didn't understood your second point but, J25 = 5V and J27 = 3.3V meaning LDO1OUT and LDO2OUT are working properly.&lt;BR /&gt;&lt;BR /&gt;Attached image is showing the D3 LED when J427 is in open position.&amp;nbsp;&lt;BR /&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 16 Feb 2024 06:31:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1809751#M31740</guid>
      <dc:creator>SParihar</dc:creator>
      <dc:date>2024-02-16T06:31:01Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in power supply to the S32K3X4-T172 board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1810271#M31760</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220636"&gt;@SParihar&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Could it be&amp;nbsp;&lt;SPAN&gt;an accidently shorted signal? Like the VDD power supply to the GND.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;J427 is responsible for voltage supply in VDD_HV_A, if there has been any overvoltage or shorting, I'm afraid there is not much that can be replicated from our side, I apologize for the inconveniences this may cause.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Julin_AragnM_0-1708121105678.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/263574i6406195749DA3ECC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Julin_AragnM_0-1708121105678.png" alt="Julin_AragnM_0-1708121105678.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Fri, 16 Feb 2024 22:07:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1810271#M31760</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-02-16T22:07:54Z</dc:date>
    </item>
    <item>
      <title>Re: Problem is power supply to the S32K3X4-T172 board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1897816#M37113</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220636"&gt;@SParihar&lt;/a&gt;&amp;nbsp;I have the same problem. Did you manage to solve this problem somehow? Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jul 2024 22:11:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/1897816#M37113</guid>
      <dc:creator>Djuric</dc:creator>
      <dc:date>2024-07-02T22:11:05Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in power supply to the S32K3X4-T172 board</title>
      <link>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/2316905#M56769</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200831"&gt;@Julián_AragónM&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I have had the same issue recently and we checked the resistor value using multimeter for P5V0 and P3V3 to the ground and it is shorted at 0-0.5 ohms whereas with another working board that we have, the value between them is well above 250 ohms&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I am assuming it is shorted, I have also followed everything in this thread and&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32DS-PEmicro-Connection-Assistant/m-p/1898602#M37155" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32DS-PEmicro-Connection-Assistant/m-p/1898602#M37155&lt;/A&gt;&amp;nbsp;thread.&lt;BR /&gt;&lt;BR /&gt;Could i receive a solution regarding this please?&lt;/P&gt;</description>
      <pubDate>Thu, 12 Feb 2026 08:06:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Problem-is-power-supply-to-the-S32K3X4-T172-board/m-p/2316905#M56769</guid>
      <dc:creator>ishoboiM</dc:creator>
      <dc:date>2026-02-12T08:06:41Z</dc:date>
    </item>
  </channel>
</rss>