<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32k3 binary flash</title>
    <link>https://community.nxp.com/t5/S32K/S32k3-binary-flash/m-p/1808937#M31712</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224860"&gt;@vikmonti7804&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Pemicro does not support raw binary files. It supports elf/hex/srec:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-download-separate-elf-srec-hex-file-to-microcontroller/ta-p/1127159" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-download-separate-elf-srec-hex-file-to-microcontroller/ta-p/1127159&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;As a workaround, you can use the same way as in example S32K344_HSE_FW_INSTALL mentioned in previous thread. The bin file is included to the project via linker file. Or use some different programmer/debugger which support this feature.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
    <pubDate>Thu, 15 Feb 2024 08:05:22 GMT</pubDate>
    <dc:creator>lukaszadrapa</dc:creator>
    <dc:date>2024-02-15T08:05:22Z</dc:date>
    <item>
      <title>S32k3 binary flash</title>
      <link>https://community.nxp.com/t5/S32K/S32k3-binary-flash/m-p/1808864#M31693</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am using the eval board S32K312EVB-Q172 with PE micro universal debugger and i want to flash the HSE fw binary to the controller but i dont see any option in s32ds which support this feature.&lt;/P&gt;&lt;P&gt;I also tried the debug configuration changes and replaced the .elf file by .bin file but its not working.&lt;/P&gt;&lt;P&gt;Can you please provide any help to flash the binary file to the controller with the debugger.&lt;/P&gt;</description>
      <pubDate>Thu, 15 Feb 2024 05:44:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k3-binary-flash/m-p/1808864#M31693</guid>
      <dc:creator>vikmonti7804</dc:creator>
      <dc:date>2024-02-15T05:44:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32k3 binary flash</title>
      <link>https://community.nxp.com/t5/S32K/S32k3-binary-flash/m-p/1808937#M31712</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224860"&gt;@vikmonti7804&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Pemicro does not support raw binary files. It supports elf/hex/srec:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-download-separate-elf-srec-hex-file-to-microcontroller/ta-p/1127159" target="_blank"&gt;https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-download-separate-elf-srec-hex-file-to-microcontroller/ta-p/1127159&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;As a workaround, you can use the same way as in example S32K344_HSE_FW_INSTALL mentioned in previous thread. The bin file is included to the project via linker file. Or use some different programmer/debugger which support this feature.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Thu, 15 Feb 2024 08:05:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k3-binary-flash/m-p/1808937#M31712</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-02-15T08:05:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32k3 binary flash</title>
      <link>https://community.nxp.com/t5/S32K/S32k3-binary-flash/m-p/1811468#M31830</link>
      <description>&lt;P&gt;Hi Lucas,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;I am trying to import a simple binary of toggle led in one of the project , there no use of hse, i just need to flash this binary with some simple code, can you please help.&amp;nbsp;&lt;/P&gt;&lt;P&gt;please fins the image of the linker file of the project which is importing the binary.&lt;/P&gt;&lt;P&gt;I need support for the code to be written in the project main function&amp;nbsp; so that program can jump to the application binary address to execute it and we can see the toggle led on the board.&lt;/P&gt;&lt;P&gt;Kindly help&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="vikmonti7804_0-1708406520124.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/263907iB497DCE3D5CDC129/image-size/medium?v=v2&amp;amp;px=400" role="button" title="vikmonti7804_0-1708406520124.png" alt="vikmonti7804_0-1708406520124.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Feb 2024 05:23:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k3-binary-flash/m-p/1811468#M31830</guid>
      <dc:creator>vikmonti7804</dc:creator>
      <dc:date>2024-02-20T05:23:32Z</dc:date>
    </item>
    <item>
      <title>Re: S32k3 binary flash</title>
      <link>https://community.nxp.com/t5/S32K/S32k3-binary-flash/m-p/1812004#M31866</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224860"&gt;@vikmonti7804&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Let me re-use text about jumping from bootloader to application I wrote earlier - see below. In addition, be aware that it's necessary to de-initialize all the features used by bootloader, especially it is necessary to disable interrupts on all levels - in the core, by local enable bits in peripherals, clear pending interrupts...&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;*********&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;In case of ARM devices&lt;/STRONG&gt;, stack pointer is initialized automatically after reset using “Initial SP value” in the vector table:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1708442530059.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/264071i302F49CC2869A49C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1708442530059.png" alt="lukaszadrapa_0-1708442530059.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;So, bootloader’s code should initialize the stack pointer as a first step and then it can jump to the application.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Here is an example from application note AN12218 S32K1xx Bootloader:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;/* Start address for the application received by the bootloader&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;* application vector table should start at this address&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;* */&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;#define APP_START_ADDRESS&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x1000&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;/**&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;* Used to jump to the entry point of the user application&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;* The Vector table of the user application must be located at 0x1000&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;*&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;* */&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;void JumpToUserApplication( unsigned int userSP,&amp;nbsp; unsigned int userStartup)&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;{&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Check if Entry address is erased and return if erased */&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(userSP == 0xFFFFFFFF){&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; return;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Set up stack pointer */&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __asm("msr msp, r0");&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __asm("msr psp, r0");&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Relocate vector table */&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; S32_SCB-&amp;gt;VTOR = (uint32_t)APP_START_ADDRESS;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Jump to application PC (r1) */&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; __asm("mov pc, r1");&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;}&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;And here is an example from application note AN12323 S32K1xx Firmware updates:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;void JumpToApplication(uint32_t start_address)&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;{&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; void (*entry)(void);&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t pc;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t __attribute__((unused)) sp;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; S32_SCB-&amp;gt;VTOR=(uint32_t)(start_address);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*Relocate interrupt table ptr*/&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; sp = *((volatile uint32_t*)start_address);&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; asm(" ldr sp, [r0,#0]");&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; pc = *((volatile uint32_t *)(start_address + 4));&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; entry = (void (*)(void))pc;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; entry();&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;}&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Feb 2024 15:23:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k3-binary-flash/m-p/1812004#M31866</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-02-20T15:23:48Z</dc:date>
    </item>
  </channel>
</rss>