<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K flash  in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K-flash/m-p/823745#M3164</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The Flash on S32K1xx can be written in 8-byte phrases.&lt;/P&gt;&lt;P&gt;Please refer to Section 36.5.11.4&amp;nbsp;Program Phrase command, RM rev.8.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 12 Aug 2018 13:23:16 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-08-12T13:23:16Z</dc:date>
    <item>
      <title>S32K flash</title>
      <link>https://community.nxp.com/t5/S32K/S32K-flash/m-p/823744#M3163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How config S32K148 P_Flash write unit to 4 Byte(in PROGRAM_LONGWORD mode)?when&amp;nbsp;I modity the macro&amp;nbsp;define &amp;nbsp;FEATURE_FLS_PF_BLOCK_WRITE_UNIT_SIZE ,FEATURE_FLS_DF_BLOCK_WRITE_UNIT_SIZE from 8 to 4 in S32K148_features.h ,but the func FLASH_DRV_Program will return STATUS_ERROR,please help me,thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Aug 2018 00:47:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-flash/m-p/823744#M3163</guid>
      <dc:creator>luo812</dc:creator>
      <dc:date>2018-08-07T00:47:11Z</dc:date>
    </item>
    <item>
      <title>Re: S32K flash</title>
      <link>https://community.nxp.com/t5/S32K/S32K-flash/m-p/823745#M3164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;The Flash on S32K1xx can be written in 8-byte phrases.&lt;/P&gt;&lt;P&gt;Please refer to Section 36.5.11.4&amp;nbsp;Program Phrase command, RM rev.8.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Aug 2018 13:23:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-flash/m-p/823745#M3164</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-08-12T13:23:16Z</dc:date>
    </item>
  </channel>
</rss>