<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32k344- ECUBUS Can Bootloader Demo-App in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32k344-ECUBUS-Can-Bootloader-Demo-App/m-p/1805089#M31592</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have different questions about the project. I am using the project of unified_bootloader but I don´t achieve the jump to application.&lt;/P&gt;&lt;P&gt;I don´t know why I have to use the vinculate file (flash).&lt;/P&gt;&lt;P&gt;I don´t know why I run the command ResetHandle in the address 0x441421 and it doesn´t jump to application and the bootloader program restarts.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the interfaz Ecubus where I have to add another application and what is the memory address and memory size?&lt;/P&gt;&lt;P&gt;Thank you for all,&lt;/P&gt;</description>
    <pubDate>Mon, 12 Feb 2024 07:17:44 GMT</pubDate>
    <dc:creator>JonAnder_Amante</dc:creator>
    <dc:date>2024-02-12T07:17:44Z</dc:date>
    <item>
      <title>S32k344- ECUBUS Can Bootloader Demo-App</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-ECUBUS-Can-Bootloader-Demo-App/m-p/1712893#M26541</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm working with S32k344 TBOX with the example&amp;nbsp;S32K344_CAN_Bootloader_RTD2d0. I want to load&amp;nbsp;S32K344_APP_Demo_RTD2d0 through ECUBUS. But I don't have clear what UDS must I send.&lt;/P&gt;&lt;P&gt;I tried with this schedule:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JosePineiro_0-1693293285413.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/238555i04C936BED087C80B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JosePineiro_0-1693293285413.png" alt="JosePineiro_0-1693293285413.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JosePineiro_0-1693293285413.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JosePineiro_1-1693293315295.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/238556i43835869D55E7513/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JosePineiro_1-1693293315295.png" alt="JosePineiro_1-1693293315295.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JosePineiro_1-1693293315295.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The result of the execution is successful but any app is loaded. I debugged and search in memory browser at flash init address defined in linker file and there are "???..."&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JosePineiro_2-1693293420292.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/238558i53EE4A371B540173/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JosePineiro_2-1693293420292.png" alt="JosePineiro_2-1693293420292.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JosePineiro_2-1693293420292.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;what may be my problem?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 07:22:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-ECUBUS-Can-Bootloader-Demo-App/m-p/1712893#M26541</guid>
      <dc:creator>JosePineiro</dc:creator>
      <dc:date>2023-08-29T07:22:50Z</dc:date>
    </item>
    <item>
      <title>Re: S32k344- ECUBUS Can Bootloader Demo-App</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-ECUBUS-Can-Bootloader-Demo-App/m-p/1713251#M26569</link>
      <description>&lt;P&gt;The last comment was resolved. I loaded ECUBUS_344CAN_uds,&amp;nbsp;S32K344_FlsDrvRTD100.bin which ones I found in the zip and&amp;nbsp;S32K344_CAN_App_RTD200.bin generated with some changes due to I'm working with S32K344 TBOX.&lt;/P&gt;&lt;P&gt;So I sent the schedule and I think the app was loaded because the debugging enter into jumptoapp and then disassembly appears in a memory address in the range of flash memory for the app.&lt;/P&gt;&lt;P&gt;My problem is that I can't load more App since ECUBUS because when the program begin to execute, jump directly to App and show that:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JosePineiro_0-1693311009164.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/238698i71FFF836020F1051/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JosePineiro_0-1693311009164.png" alt="JosePineiro_0-1693311009164.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JosePineiro_0-1693311009164.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I tried to power reset but I don´t know what is the problem. Other UDS schedule are necessary for load a new application and regret from App to Boot?&lt;/P&gt;</description>
      <pubDate>Tue, 29 Aug 2023 12:13:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-ECUBUS-Can-Bootloader-Demo-App/m-p/1713251#M26569</guid>
      <dc:creator>JosePineiro</dc:creator>
      <dc:date>2023-08-29T12:13:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32k344- ECUBUS Can Bootloader Demo-App</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-ECUBUS-Can-Bootloader-Demo-App/m-p/1805089#M31592</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have different questions about the project. I am using the project of unified_bootloader but I don´t achieve the jump to application.&lt;/P&gt;&lt;P&gt;I don´t know why I have to use the vinculate file (flash).&lt;/P&gt;&lt;P&gt;I don´t know why I run the command ResetHandle in the address 0x441421 and it doesn´t jump to application and the bootloader program restarts.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the interfaz Ecubus where I have to add another application and what is the memory address and memory size?&lt;/P&gt;&lt;P&gt;Thank you for all,&lt;/P&gt;</description>
      <pubDate>Mon, 12 Feb 2024 07:17:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-ECUBUS-Can-Bootloader-Demo-App/m-p/1805089#M31592</guid>
      <dc:creator>JonAnder_Amante</dc:creator>
      <dc:date>2024-02-12T07:17:44Z</dc:date>
    </item>
    <item>
      <title>Re: S32k344- ECUBUS Can Bootloader Demo-App</title>
      <link>https://community.nxp.com/t5/S32K/S32k344-ECUBUS-Can-Bootloader-Demo-App/m-p/1840621#M33798</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am using the project "S32K344_Can_bootloader_RTD200" in the microprocessor S32K344. I want to download an application with the program of bootloader. I have achieved the jump from program to application but I have different questions.&lt;/P&gt;&lt;P&gt;1. I want to use #define EN_DELAY_TIME but when I uncomment the command in the folder "public_inc", the program has different errors. My target to use "Backdoor", that is to say, I want to check if the program has to enter to bootloader or not. I don´t know the process and the different functions that I have to use to achieve the target. I want to use the function "Boot_CheckReqBootloaderMode(void)" but when I debug the program, it never enters to the "if". Could you explain me the process and the steps to achieve the target. I add different functions that I think are important.&amp;nbsp;&lt;/P&gt;&lt;P&gt;2. I don´t know if I have to modificate the parameters of "static tJumpAppDelayTimeInfo gs_stJumpAPPDelayTimeInfo = {FALSE, 0u};". I have to change this structure ? You can see all structure in one of the next pictures.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need the reply as soon as possible since I have to send a project very soon.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_0-1712229623375.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/271956iDD345D0C3DA198F4/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_0-1712229623375.png" alt="JonAnder_Amante_0-1712229623375.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JonAnder_Amante_0-1712229623375.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_1-1712229623606.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/271957i631123CD8540B7D0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_1-1712229623606.png" alt="JonAnder_Amante_1-1712229623606.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JonAnder_Amante_1-1712229623606.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_2-1712229623614.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/271958i72289ACAFC2ECF24/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_2-1712229623614.png" alt="JonAnder_Amante_2-1712229623614.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JonAnder_Amante_2-1712229623614.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_3-1712229623617.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/271960i8A5F3AB498786107/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_3-1712229623617.png" alt="JonAnder_Amante_3-1712229623617.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JonAnder_Amante_3-1712229623617.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JonAnder_Amante_4-1712229623604.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/271959iB73990C88E2C20BF/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JonAnder_Amante_4-1712229623604.png" alt="JonAnder_Amante_4-1712229623604.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JonAnder_Amante_4-1712229623604.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for all,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Jon Ander Amante Jorge&lt;/P&gt;</description>
      <pubDate>Thu, 04 Apr 2024 11:20:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32k344-ECUBUS-Can-Bootloader-Demo-App/m-p/1840621#M33798</guid>
      <dc:creator>JonAnder_Amante</dc:creator>
      <dc:date>2024-04-04T11:20:36Z</dc:date>
    </item>
  </channel>
</rss>