<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: S32K144 FlexCAN Clock Options</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Clock-Options/m-p/823145#M3156</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Damien,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think text in chapter 53.1.6 is complete.&lt;/P&gt;&lt;P&gt;However used clock terms in whole FlexCAN chapter could be little bit misguiding.&lt;/P&gt;&lt;P&gt;The protocol engine clock (PE clock, CANCLK), that is used for CAN bit timing specification, can be connected either to Oscillator clock or to Peripheral clock, selected by CTRL1[CLKSRC] bit.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70410i20C6E6782C00CB12/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The chapter 53.1.6 describe just the Oscillator Clock source, which is SOSCDIV2_CLK in this device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Peripheral clock is not specified this way and it is only visible from Table 27-9 and it is SYS_CLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Aug 2018 10:48:00 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2018-08-28T10:48:00Z</dc:date>
    <item>
      <title>S32K144 FlexCAN Clock Options</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Clock-Options/m-p/823144#M3155</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would just like to query what appears to be an inconsistency in the reference manual (Rev 8 06/2018) for the S32K144.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In Section 53.1.6 on Page 1631, it says that "FlexCAN oscillator clock is SOSCDIV2_CLK as mentioned in section Table 27-9"&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67509i0CCA0A861CE9613B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Whereas Table 27-9 on 9547 (and the clock config tool in AN5408), the peripheral clock is able to be switched between the SYS_CLK and the SOSCDIV2_CLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/67553i7E62D54054B9BA2A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Can I please confirm that the text in s53.1.6 is incomplete?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Damien.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Aug 2018 08:17:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Clock-Options/m-p/823144#M3155</guid>
      <dc:creator>damiendusha</dc:creator>
      <dc:date>2018-08-24T08:17:40Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 FlexCAN Clock Options</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Clock-Options/m-p/823145#M3156</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Damien,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think text in chapter 53.1.6 is complete.&lt;/P&gt;&lt;P&gt;However used clock terms in whole FlexCAN chapter could be little bit misguiding.&lt;/P&gt;&lt;P&gt;The protocol engine clock (PE clock, CANCLK), that is used for CAN bit timing specification, can be connected either to Oscillator clock or to Peripheral clock, selected by CTRL1[CLKSRC] bit.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/70410i20C6E6782C00CB12/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The chapter 53.1.6 describe just the Oscillator Clock source, which is SOSCDIV2_CLK in this device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Peripheral clock is not specified this way and it is only visible from Table 27-9 and it is SYS_CLK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Aug 2018 10:48:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-FlexCAN-Clock-Options/m-p/823145#M3156</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2018-08-28T10:48:00Z</dc:date>
    </item>
  </channel>
</rss>