<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: FlexCAN bus error handling?</title>
    <link>https://community.nxp.com/t5/S32K/FlexCAN-bus-error-handling/m-p/1804145#M31551</link>
    <description>&lt;P&gt;Thanks PetrS &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 08 Feb 2024 14:19:07 GMT</pubDate>
    <dc:creator>reymor</dc:creator>
    <dc:date>2024-02-08T14:19:07Z</dc:date>
    <item>
      <title>FlexCAN bus error handling?</title>
      <link>https://community.nxp.com/t5/S32K/FlexCAN-bus-error-handling/m-p/1802120#M31457</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;We use&lt;/P&gt;&lt;P&gt;- S32K144W&lt;/P&gt;&lt;P&gt;- S32DS 3.3&lt;/P&gt;&lt;P&gt;- SDK RTM 4.0.1&lt;/P&gt;&lt;P&gt;- CAN without FD&lt;/P&gt;&lt;P&gt;Maybe this is something wrong, but in which context &lt;STRONG&gt;CANx_Error_IRQHandler &lt;/STRONG&gt;is called?&lt;/P&gt;&lt;P&gt;Is there any example for handling CAN bus errors using the FlexCan driver?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Basically, we disconnect the CAN bus which means an aknowledge error, but it is never called. We have introduced error in the bus and this fuctions is never called&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="reymor_0-1707164791092.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/262006iBBE6D72B8C4036B0/image-size/medium?v=v2&amp;amp;px=400" role="button" title="reymor_0-1707164791092.png" alt="reymor_0-1707164791092.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;We saw that in&amp;nbsp;FLEXCAN_EnableIRQs::L617 the IRQ is enabled. However, we are not sure in which context&amp;nbsp;&lt;STRONG&gt;CANx_Error_IRQHandler &lt;/STRONG&gt;is called&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 05 Feb 2024 20:31:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlexCAN-bus-error-handling/m-p/1802120#M31457</guid>
      <dc:creator>reymor</dc:creator>
      <dc:date>2024-02-05T20:31:50Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN bus error handling?</title>
      <link>https://community.nxp.com/t5/S32K/FlexCAN-bus-error-handling/m-p/1802608#M31483</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;I tested error interrupt/callback using below example, I posted. It is using older SDK, but it should be similar, I guess.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-FlexCAN-TX-RX-Error-ISR-test-S32DS2-2/ta-p/1278224" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K144-FlexCAN-TX-RX-Error-ISR-test-S32DS2-2/ta-p/1278224&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;</description>
      <pubDate>Tue, 06 Feb 2024 11:07:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlexCAN-bus-error-handling/m-p/1802608#M31483</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-02-06T11:07:44Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCAN bus error handling?</title>
      <link>https://community.nxp.com/t5/S32K/FlexCAN-bus-error-handling/m-p/1804145#M31551</link>
      <description>&lt;P&gt;Thanks PetrS &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Feb 2024 14:19:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/FlexCAN-bus-error-handling/m-p/1804145#M31551</guid>
      <dc:creator>reymor</dc:creator>
      <dc:date>2024-02-08T14:19:07Z</dc:date>
    </item>
  </channel>
</rss>