<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックFlash selected memory sections</title>
    <link>https://community.nxp.com/t5/S32K/Flash-selected-memory-sections/m-p/1801867#M31449</link>
    <description>&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;is it possible to flash only selected memory sections of the S32K358?&lt;/P&gt;&lt;P&gt;Let's say we have two different projects that use one core each and we only want to update the code of core 2 (i.e. progam the .elf of project 2 but not delete the existing code/data of core 0).&lt;/P&gt;&lt;P&gt;I was unable to find any specific settings in the debug configurations.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Mon, 05 Feb 2024 12:16:36 GMT</pubDate>
    <dc:creator>Iota</dc:creator>
    <dc:date>2024-02-05T12:16:36Z</dc:date>
    <item>
      <title>Flash selected memory sections</title>
      <link>https://community.nxp.com/t5/S32K/Flash-selected-memory-sections/m-p/1801867#M31449</link>
      <description>&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;is it possible to flash only selected memory sections of the S32K358?&lt;/P&gt;&lt;P&gt;Let's say we have two different projects that use one core each and we only want to update the code of core 2 (i.e. progam the .elf of project 2 but not delete the existing code/data of core 0).&lt;/P&gt;&lt;P&gt;I was unable to find any specific settings in the debug configurations.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Mon, 05 Feb 2024 12:16:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flash-selected-memory-sections/m-p/1801867#M31449</guid>
      <dc:creator>Iota</dc:creator>
      <dc:date>2024-02-05T12:16:36Z</dc:date>
    </item>
    <item>
      <title>Re: Flash selected memory sections</title>
      <link>https://community.nxp.com/t5/S32K/Flash-selected-memory-sections/m-p/1803580#M31527</link>
      <description>&lt;P&gt;It is possible. It is needed to have configuration with more ELF or S-record files (one for each core) and these files use only certain range of addresses.&lt;/P&gt;
&lt;P&gt;Some debuggers program only these flash sectors which differ from MCU flash content (for instance TRACE32).&lt;/P&gt;
&lt;P&gt;With S32DS and PeMicro debugger it is possible to preserve certain address ranges (it performs read-modify-write operation) as on the screenshot below:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="davidtosenovjan_0-1707328868694.png" style="width: 508px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/262379i377EB548E9EFEB80/image-dimensions/508x579?v=v2" width="508" height="579" role="button" title="davidtosenovjan_0-1707328868694.png" alt="davidtosenovjan_0-1707328868694.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;davidtosenovjan_0-1707328868694.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Feb 2024 18:01:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flash-selected-memory-sections/m-p/1803580#M31527</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2024-02-07T18:01:23Z</dc:date>
    </item>
  </channel>
</rss>