<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic [S32K324] What's the max frequency of the CLKOUT_RUN_CLK in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K324-What-s-the-max-frequency-of-the-CLKOUT-RUN-CLK/m-p/1801664#M31436</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the CLKOUT_RUN function, eg, using the PTB5, to output the tested clock source.&lt;/P&gt;&lt;P&gt;But I find that the&amp;nbsp; CLKOUT_RUN_CLK can't output about over 20Mhz, right?&lt;/P&gt;&lt;P&gt;I don't find information from the RM or DS about the&amp;nbsp;max frequency of the CLKOUT_RUN_CLK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you help me check that?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Gavin&lt;/P&gt;</description>
    <pubDate>Mon, 05 Feb 2024 06:46:46 GMT</pubDate>
    <dc:creator>GavinLi1</dc:creator>
    <dc:date>2024-02-05T06:46:46Z</dc:date>
    <item>
      <title>[S32K324] What's the max frequency of the CLKOUT_RUN_CLK</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-What-s-the-max-frequency-of-the-CLKOUT-RUN-CLK/m-p/1801664#M31436</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using the CLKOUT_RUN function, eg, using the PTB5, to output the tested clock source.&lt;/P&gt;&lt;P&gt;But I find that the&amp;nbsp; CLKOUT_RUN_CLK can't output about over 20Mhz, right?&lt;/P&gt;&lt;P&gt;I don't find information from the RM or DS about the&amp;nbsp;max frequency of the CLKOUT_RUN_CLK.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you help me check that?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Gavin&lt;/P&gt;</description>
      <pubDate>Mon, 05 Feb 2024 06:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-What-s-the-max-frequency-of-the-CLKOUT-RUN-CLK/m-p/1801664#M31436</guid>
      <dc:creator>GavinLi1</dc:creator>
      <dc:date>2024-02-05T06:46:46Z</dc:date>
    </item>
    <item>
      <title>Re: [S32K324] What's the max frequency of the CLKOUT_RUN_CLK</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-What-s-the-max-frequency-of-the-CLKOUT-RUN-CLK/m-p/1803397#M31523</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;PTB5 is a GPIO-STANDARD-PLUS pad (See IOMUX spreadsheet), meaning it can only be driven at a maximum of 25MHz. (Section 4.4.1 of the RM)&lt;/P&gt;
&lt;P&gt;You should be able to drive faster speeds out of PTD10 (GPIO-FAST, Up to 120MHz switching according to the same chapter of RM)&lt;/P&gt;
&lt;P&gt;The reason is there are a limited number of medium/fast pads on S32K3, and on the eval board most of these are routed to high-speed interfaces such as Ethernet or QSPI&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Wed, 07 Feb 2024 13:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-What-s-the-max-frequency-of-the-CLKOUT-RUN-CLK/m-p/1803397#M31523</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2024-02-07T13:37:07Z</dc:date>
    </item>
  </channel>
</rss>