<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Sample code for interfacing four MC33774 with S32K312 Microcontroller in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Sample-code-for-interfacing-four-MC33774-with-S32K312/m-p/1800044#M31335</link>
    <description>&lt;P&gt;In our new project we have a hardware configuration with S32K312 controller interfaces to MC33664 and then TPL communication will be connected to four MC33774.&amp;nbsp;&lt;/P&gt;&lt;P&gt;To quick start the project, would like to check if there is any application note or source code available to interface between&amp;nbsp;&amp;nbsp;S32K312 -&amp;gt;&amp;nbsp;MC33664 -&amp;gt;&amp;nbsp;MC33774&lt;/P&gt;</description>
    <pubDate>Thu, 01 Feb 2024 15:27:13 GMT</pubDate>
    <dc:creator>amattanchery</dc:creator>
    <dc:date>2024-02-01T15:27:13Z</dc:date>
    <item>
      <title>Sample code for interfacing four MC33774 with S32K312 Microcontroller</title>
      <link>https://community.nxp.com/t5/S32K/Sample-code-for-interfacing-four-MC33774-with-S32K312/m-p/1800044#M31335</link>
      <description>&lt;P&gt;In our new project we have a hardware configuration with S32K312 controller interfaces to MC33664 and then TPL communication will be connected to four MC33774.&amp;nbsp;&lt;/P&gt;&lt;P&gt;To quick start the project, would like to check if there is any application note or source code available to interface between&amp;nbsp;&amp;nbsp;S32K312 -&amp;gt;&amp;nbsp;MC33664 -&amp;gt;&amp;nbsp;MC33774&lt;/P&gt;</description>
      <pubDate>Thu, 01 Feb 2024 15:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Sample-code-for-interfacing-four-MC33774-with-S32K312/m-p/1800044#M31335</guid>
      <dc:creator>amattanchery</dc:creator>
      <dc:date>2024-02-01T15:27:13Z</dc:date>
    </item>
    <item>
      <title>Re: Sample code for interfacing four MC33774 with S32K312 Microcontroller</title>
      <link>https://community.nxp.com/t5/S32K/Sample-code-for-interfacing-four-MC33774-with-S32K312/m-p/1800270#M31342</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196767"&gt;@amattanchery&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The available information about the MC33774/MC33664&amp;nbsp;with S32K3 is related to&amp;nbsp;Battery Management Unit solutions, which is under NDA&amp;nbsp;(Non-Disclosure Agreement) the information is not public, and we can not share the information due to the security levels when working with an automotive part such as this. Contact your NXP representative for further support in this part.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R.&lt;/P&gt;
&lt;P&gt;VaneB&lt;/P&gt;</description>
      <pubDate>Thu, 01 Feb 2024 20:50:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Sample-code-for-interfacing-four-MC33774-with-S32K312/m-p/1800270#M31342</guid>
      <dc:creator>VaneB</dc:creator>
      <dc:date>2024-02-01T20:50:02Z</dc:date>
    </item>
  </channel>
</rss>