<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K344 CAN can't send Message in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1799667#M31312</link>
    <description>&lt;P&gt;&lt;STRONG&gt;&lt;SPAN&gt;&lt;A href="https://infopulsepro.com/" target="_self"&gt;Infopulsepro&lt;/A&gt;@&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Check CAN Transceiver Connections&lt;/STRONG&gt;: Ensure that the CAN transceiver is properly connected to the S32K344 microcontroller. Verify that the CAN_H and CAN_L lines are connected correctly and that the transceiver is powered appropriately.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Verify CAN Controller Configuration&lt;/STRONG&gt;: Double-check the configuration of the S32K344 CAN controller registers. Ensure that the baud rate, timing parameters, and other settings are correctly set according to your CAN network requirements.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Check Error Flags&lt;/STRONG&gt;: Monitor the CAN error flags to determine if there are any issues detected by the CAN controller. Common error flags include bit stuffing errors, CRC errors, form errors, and ACK errors. Clear any error flags and observe if they reappear during message transmission.&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;</description>
    <pubDate>Thu, 01 Feb 2024 08:22:47 GMT</pubDate>
    <dc:creator>Emily54</dc:creator>
    <dc:date>2024-02-01T08:22:47Z</dc:date>
    <item>
      <title>S32K344 CAN can't send Message</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1255661#M10417</link>
      <description>I am using S32K344 and New "FlexCAN_example_CT(SDK version: RTD 0.9.0 D2013)",Update the code after modifying the CAN0 IO configuration.But CAN0 did not send any information, use the oscilloscope to check the CAN0 PTA6 level and there is no change.After checking the code, I found that the updated code did not add IO initialization information, so I added the function Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS0,g_pin_mux_InitConfigArr0).It still doesn't work after adding IO initialization.</description>
      <pubDate>Thu, 01 Apr 2021 08:34:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1255661#M10417</guid>
      <dc:creator>longfeiwang</dc:creator>
      <dc:date>2021-04-01T08:34:28Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN can't send Message</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1257258#M10453</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/138254"&gt;@longfeiwang&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Could you please share the project so that I can test it?&lt;/P&gt;
&lt;P&gt;PTA6 is a CAN0_RX pin.&lt;/P&gt;
&lt;P&gt;Have you read the corresponding MSCRn registers of the TX, RX pins after the initialization?&lt;/P&gt;
&lt;P&gt;Were the correct source signal selected in the registers?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 06 Apr 2021 10:19:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1257258#M10453</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-04-06T10:19:22Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN can't send Message</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1257604#M10463</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Daniel&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&amp;nbsp;The IO configuration is shown in the figure below:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="longfeiwang_2-1617762787495.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/141457i632815F27F492ECE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="longfeiwang_2-1617762787495.png" alt="longfeiwang_2-1617762787495.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Apr 2021 02:34:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1257604#M10463</guid>
      <dc:creator>longfeiwang</dc:creator>
      <dc:date>2021-04-07T02:34:06Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN can't send Message</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1260439#M10515</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/138254"&gt;@longfeiwang&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I'm sorry for the delay,&lt;/P&gt;
&lt;P&gt;You haven't changed the FlexCAN mode: &lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_0-1618218543771.png" style="width: 571px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/142011i7B3202FBE1546EEA/image-dimensions/571x290?v=v2" width="571" height="290" role="button" title="danielmartynek_0-1618218543771.png" alt="danielmartynek_0-1618218543771.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please have a look at the description of the FlexCAN modes in the S32K3xx RM:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielmartynek_1-1618218623079.png" style="width: 740px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/142012iFAFC26346C890AC0/image-dimensions/740x134?v=v2" width="740" height="134" role="button" title="danielmartynek_1-1618218623079.png" alt="danielmartynek_1-1618218623079.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Apr 2021 09:11:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1260439#M10515</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2021-04-12T09:11:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN can't send Message</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1798727#M31277</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I am also using same controller s32k344 following is the example that I am attaching. I was getting the same issue as @longfeiwang ,so like you said I disabled the loopback.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="avinashstarkenn_0-1706706349029.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/261073iC505E13FB0248D92/image-size/medium?v=v2&amp;amp;px=400" role="button" title="avinashstarkenn_0-1706706349029.png" alt="avinashstarkenn_0-1706706349029.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But now it is not transmitting and not entering CanIf_TxConfirmation function which confirms Transmission is done.&lt;/P&gt;&lt;P&gt;Please resolve the issue as soon as possible&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 13:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1798727#M31277</guid>
      <dc:creator>avinashstarkenn</dc:creator>
      <dc:date>2024-01-31T13:08:37Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN can't send Message</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1798752#M31278</link>
      <description>&lt;P&gt;HI &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221165"&gt;@avinashstarkenn&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Can you please create a new thread?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you,&lt;/P&gt;
&lt;P&gt;BR, Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 13:32:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1798752#M31278</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-01-31T13:32:24Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN can't send Message</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1799518#M31303</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;As my issue is same please resolve the issue here.&lt;/P&gt;&lt;P&gt;Please do it as soon as possible.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Feb 2024 05:42:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1799518#M31303</guid>
      <dc:creator>avinashstarkenn</dc:creator>
      <dc:date>2024-02-01T05:42:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN can't send Message</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1799667#M31312</link>
      <description>&lt;P&gt;&lt;STRONG&gt;&lt;SPAN&gt;&lt;A href="https://infopulsepro.com/" target="_self"&gt;Infopulsepro&lt;/A&gt;@&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Check CAN Transceiver Connections&lt;/STRONG&gt;: Ensure that the CAN transceiver is properly connected to the S32K344 microcontroller. Verify that the CAN_H and CAN_L lines are connected correctly and that the transceiver is powered appropriately.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Verify CAN Controller Configuration&lt;/STRONG&gt;: Double-check the configuration of the S32K344 CAN controller registers. Ensure that the baud rate, timing parameters, and other settings are correctly set according to your CAN network requirements.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Check Error Flags&lt;/STRONG&gt;: Monitor the CAN error flags to determine if there are any issues detected by the CAN controller. Common error flags include bit stuffing errors, CRC errors, form errors, and ACK errors. Clear any error flags and observe if they reappear during message transmission.&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;</description>
      <pubDate>Thu, 01 Feb 2024 08:22:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1799667#M31312</guid>
      <dc:creator>Emily54</dc:creator>
      <dc:date>2024-02-01T08:22:47Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN can't send Message</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1799716#M31320</link>
      <description>&lt;P&gt;Please look into the code and give me specific solution. You are giving me generic debugging method&lt;/P&gt;</description>
      <pubDate>Thu, 01 Feb 2024 09:03:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1799716#M31320</guid>
      <dc:creator>avinashstarkenn</dc:creator>
      <dc:date>2024-02-01T09:03:55Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 CAN can't send Message</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1801772#M31440</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;DIV&gt;see attached modified code. It sends message with std ID 0x1 first then wait for message with std ID 0x2, once received it send ID 0x1 message back with incrementing first byte in payload.&lt;/DIV&gt;
&lt;DIV&gt;This what I see with PCAN connected on S32K3x4EVB-Q172 board (rev.A).&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="PetrS_0-1707124263572.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/261927i374DEE1AE6FFA4E6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="PetrS_0-1707124263572.png" alt="PetrS_0-1707124263572.png" /&gt;&lt;/span&gt;
&lt;P&gt;But I gave you this already within a Case you created.&lt;/P&gt;
&lt;P&gt;BR, Petr&lt;/P&gt;
&lt;/DIV&gt;</description>
      <pubDate>Mon, 05 Feb 2024 09:13:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-CAN-can-t-send-Message/m-p/1801772#M31440</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2024-02-05T09:13:21Z</dc:date>
    </item>
  </channel>
</rss>