<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K324 Quadrature Decode</title>
    <link>https://community.nxp.com/t5/S32K/S32K324-Quadrature-Decode/m-p/1796158#M31129</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In my application I have realised the acquisition of a quadrature signal by following all the instructions in Application Note AN13884 and it works.&lt;/P&gt;&lt;P&gt;Now I wanted to acquire another quadrature signal but unlike the previous case and as described in the application note one of the two pins cannot be connected to the TRGMUX and therefore I cannot apply the chain TRGMUX -&amp;gt; LCU1 -&amp;gt; TRGMUX -&amp;gt; EMIOS1.&lt;BR /&gt;In particular, the pins I use are PTA20 and PTC27 and the pin in question is PTC27.&lt;BR /&gt;I wanted to know how to exploit this pin to apply the same logic described in the example.&lt;/P&gt;&lt;P&gt;MCU S32K24&lt;BR /&gt;IDE S32 Design Studio 3.5&lt;BR /&gt;RTD 3.0.0&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;</description>
    <pubDate>Fri, 26 Jan 2024 16:15:58 GMT</pubDate>
    <dc:creator>Simone9</dc:creator>
    <dc:date>2024-01-26T16:15:58Z</dc:date>
    <item>
      <title>S32K324 Quadrature Decode</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-Quadrature-Decode/m-p/1796158#M31129</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;In my application I have realised the acquisition of a quadrature signal by following all the instructions in Application Note AN13884 and it works.&lt;/P&gt;&lt;P&gt;Now I wanted to acquire another quadrature signal but unlike the previous case and as described in the application note one of the two pins cannot be connected to the TRGMUX and therefore I cannot apply the chain TRGMUX -&amp;gt; LCU1 -&amp;gt; TRGMUX -&amp;gt; EMIOS1.&lt;BR /&gt;In particular, the pins I use are PTA20 and PTC27 and the pin in question is PTC27.&lt;BR /&gt;I wanted to know how to exploit this pin to apply the same logic described in the example.&lt;/P&gt;&lt;P&gt;MCU S32K24&lt;BR /&gt;IDE S32 Design Studio 3.5&lt;BR /&gt;RTD 3.0.0&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Jan 2024 16:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-Quadrature-Decode/m-p/1796158#M31129</guid>
      <dc:creator>Simone9</dc:creator>
      <dc:date>2024-01-26T16:15:58Z</dc:date>
    </item>
    <item>
      <title>Re: S32K324 Quadrature Decode</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-Quadrature-Decode/m-p/1796779#M31162</link>
      <description>&lt;P&gt;Hi Simone,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;In order to bring encoder phase signal to the LCU for preprocessing, a PIN with&amp;nbsp;&amp;nbsp;TRGMUX_IN functionality is needed.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas Fedor.&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jan 2024 09:54:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-Quadrature-Decode/m-p/1796779#M31162</guid>
      <dc:creator>tomasfedor</dc:creator>
      <dc:date>2024-01-29T09:54:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K324 Quadrature Decode</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-Quadrature-Decode/m-p/1796796#M31163</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;BR /&gt;I can't change the pin for allow this connection.&lt;BR /&gt;In any way, it is possible to perform quadrature decode using only the eMIOS without LCU?&lt;BR /&gt;&lt;BR /&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jan 2024 10:06:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-Quadrature-Decode/m-p/1796796#M31163</guid>
      <dc:creator>Simone9</dc:creator>
      <dc:date>2024-01-29T10:06:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K324 Quadrature Decode</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-Quadrature-Decode/m-p/1796800#M31164</link>
      <description>&lt;P&gt;Hi Simone,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;No, In order to perform quadrature decoder functionality, eMIOS needs preprocessed signals by LCU on S32K324.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Tomas Fedor.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jan 2024 10:19:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-Quadrature-Decode/m-p/1796800#M31164</guid>
      <dc:creator>tomasfedor</dc:creator>
      <dc:date>2024-01-29T10:19:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32K324 Quadrature Decode</title>
      <link>https://community.nxp.com/t5/S32K/S32K324-Quadrature-Decode/m-p/2354369#M58107</link>
      <description>&lt;P&gt;Is there a quadrature decode example made for MBDT? I can make the configuration in the S32 Configuration tool, but I want to know how to read the data in Simulink&lt;/P&gt;</description>
      <pubDate>Tue, 21 Apr 2026 20:53:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K324-Quadrature-Decode/m-p/2354369#M58107</guid>
      <dc:creator>MarcoRdzGmz</dc:creator>
      <dc:date>2026-04-21T20:53:06Z</dc:date>
    </item>
  </channel>
</rss>