<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: Flex CAN Message buffer Configuration</title>
    <link>https://community.nxp.com/t5/S32K/Flex-CAN-Message-buffer-Configuration/m-p/819692#M3098</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;even if you set the memory buffer area to 64 payload, you can easily send 8 bytes only, just set the MB's DLC (Data Length Code) properly. Of course you have less number of MBs available.&lt;/P&gt;&lt;P&gt;If the payload configuration is changed using&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;FDCTRL.MBDSR0, starting address of each MB is different, so you must be sure correct addresses are used. You can refer to chapter 53.4.5 of the RM for a MB's memory map for each payload configuration.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Do you use SDK driver or some own code?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;BR, Petr&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Jan 2019 11:15:36 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2019-01-04T11:15:36Z</dc:date>
    <item>
      <title>Flex CAN Message buffer Configuration</title>
      <link>https://community.nxp.com/t5/S32K/Flex-CAN-Message-buffer-Configuration/m-p/819691#M3097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have an NXP S32K142 EVB board. I had a code which works fine In FD mode with 64 bytes message configuration.&lt;/P&gt;&lt;P&gt;When I tried to configure the message buffer to 8 bytes or less than 64 bytes I couldn't see transmit signal in oscilloscope.&lt;/P&gt;&lt;P&gt;The change I made is configuring the FDCTRL.MBDSR0 = 00 to make message buffer as 8byte size. Is there any thing more to update to configure for 8 byte message buffer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Satheesh.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Dec 2018 06:42:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flex-CAN-Message-buffer-Configuration/m-p/819691#M3097</guid>
      <dc:creator>satheesh_mb</dc:creator>
      <dc:date>2018-12-20T06:42:22Z</dc:date>
    </item>
    <item>
      <title>Re: Flex CAN Message buffer Configuration</title>
      <link>https://community.nxp.com/t5/S32K/Flex-CAN-Message-buffer-Configuration/m-p/819692#M3098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;even if you set the memory buffer area to 64 payload, you can easily send 8 bytes only, just set the MB's DLC (Data Length Code) properly. Of course you have less number of MBs available.&lt;/P&gt;&lt;P&gt;If the payload configuration is changed using&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;FDCTRL.MBDSR0, starting address of each MB is different, so you must be sure correct addresses are used. You can refer to chapter 53.4.5 of the RM for a MB's memory map for each payload configuration.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Do you use SDK driver or some own code?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;BR, Petr&amp;nbsp;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2019 11:15:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Flex-CAN-Message-buffer-Configuration/m-p/819692#M3098</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2019-01-04T11:15:36Z</dc:date>
    </item>
  </channel>
</rss>