<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K358 WIFI module 88w8897 function test</title>
    <link>https://community.nxp.com/t5/S32K/S32K358-WIFI-module-88w8897-function-test/m-p/1793470#M30964</link>
    <description>&lt;P&gt;&amp;nbsp;Hi，&lt;/P&gt;&lt;P&gt;I have encountered three problems while developing the wifi &amp;amp;bt bluetooth functions of the s32k358 sdhc:&lt;BR /&gt;1. sdhc initialization failed: call uSDHC_Init() function returns false&lt;BR /&gt;2. uart1 can not run normally, the program uses uart1, but we use all the pins of lpuart1 to send PTA18/PTB22/PTC7/PTC9/PTD14, and receive pins: PTA19/PTB23/PTC6/PTC8/PTD13, are unable to realize the receive and send function of Lpuart1. The Lpuart1 can't receive and transmit, i.e., it can't send and receive information in the pc serial port tool.&lt;BR /&gt;3. Is there any test manual for this wifi module 88W8987? What commands need to be sent through the serial port to make the wifi work?&lt;/P&gt;&lt;P&gt;The information about the platform we are using is as follows:&lt;BR /&gt;Package: sdhc_wifi_S32K358, installation version S32K3_SDHC_CD1_0_4_0_D2307_updatesite.zip&lt;BR /&gt;RTD version: 3.0.0&lt;BR /&gt;wifi&amp;amp;bt module: 88W8987, Ublox module used: JODY-W263-01A&lt;BR /&gt;Hardware board: s32k358 development board bought from Taobao.&lt;/P&gt;&lt;P&gt;Would you like to analyze and solve this problem, I am looking forward to your reply.thanks!&lt;/P&gt;</description>
    <pubDate>Tue, 23 Jan 2024 05:51:14 GMT</pubDate>
    <dc:creator>xiaojinlong</dc:creator>
    <dc:date>2024-01-23T05:51:14Z</dc:date>
    <item>
      <title>S32K358 WIFI module 88w8897 function test</title>
      <link>https://community.nxp.com/t5/S32K/S32K358-WIFI-module-88w8897-function-test/m-p/1793470#M30964</link>
      <description>&lt;P&gt;&amp;nbsp;Hi，&lt;/P&gt;&lt;P&gt;I have encountered three problems while developing the wifi &amp;amp;bt bluetooth functions of the s32k358 sdhc:&lt;BR /&gt;1. sdhc initialization failed: call uSDHC_Init() function returns false&lt;BR /&gt;2. uart1 can not run normally, the program uses uart1, but we use all the pins of lpuart1 to send PTA18/PTB22/PTC7/PTC9/PTD14, and receive pins: PTA19/PTB23/PTC6/PTC8/PTD13, are unable to realize the receive and send function of Lpuart1. The Lpuart1 can't receive and transmit, i.e., it can't send and receive information in the pc serial port tool.&lt;BR /&gt;3. Is there any test manual for this wifi module 88W8987? What commands need to be sent through the serial port to make the wifi work?&lt;/P&gt;&lt;P&gt;The information about the platform we are using is as follows:&lt;BR /&gt;Package: sdhc_wifi_S32K358, installation version S32K3_SDHC_CD1_0_4_0_D2307_updatesite.zip&lt;BR /&gt;RTD version: 3.0.0&lt;BR /&gt;wifi&amp;amp;bt module: 88W8987, Ublox module used: JODY-W263-01A&lt;BR /&gt;Hardware board: s32k358 development board bought from Taobao.&lt;/P&gt;&lt;P&gt;Would you like to analyze and solve this problem, I am looking forward to your reply.thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 23 Jan 2024 05:51:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K358-WIFI-module-88w8897-function-test/m-p/1793470#M30964</guid>
      <dc:creator>xiaojinlong</dc:creator>
      <dc:date>2024-01-23T05:51:14Z</dc:date>
    </item>
  </channel>
</rss>