<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: Low power Timer issue</title>
    <link>https://community.nxp.com/t5/S32K/Low-power-Timer-issue/m-p/628806#M309</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried your code on two boards and it works on the new S32K144EVB-Q100 with N47T. But it doesn’t work on FRDMPK144-Q100 with N77P. I have rewritten the code without SDK, but it doesn’t work either. Although the flag is set, it won’t go into ISR. The problem is in the N77P mask set which is a prototype. &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Feb 2017 07:48:32 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2017-02-22T07:48:32Z</dc:date>
    <item>
      <title>Low power Timer issue</title>
      <link>https://community.nxp.com/t5/S32K/Low-power-Timer-issue/m-p/628803#M306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How to use LPT two channels?&lt;/P&gt;&lt;P&gt;One channel is ok, but add two, it can't jump to interrupt function, pls help check it.&lt;/P&gt;&lt;P&gt;Also it alwayls show errors, but image file is generated, pls see the attached example and picture.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338873"&gt;LowPTimer.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Feb 2017 08:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Low-power-Timer-issue/m-p/628803#M306</guid>
      <dc:creator>huaping</dc:creator>
      <dc:date>2017-02-13T08:44:09Z</dc:date>
    </item>
    <item>
      <title>Re: Low power Timer issue</title>
      <link>https://community.nxp.com/t5/S32K/Low-power-Timer-issue/m-p/628804#M307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In ISR of channel 1 you clear TIF2(Channel 2 Timer Interrupt Flag)&lt;/P&gt;&lt;P&gt;LPIT_DRV_ClearInterruptFlagTimerChannels(FSL_LPIT1, (1 &amp;lt;&amp;lt;2));&amp;nbsp; // Should be (1 &amp;lt;&amp;lt; 1)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I didn’t get any error when I built your project. Have you tried cleaning the project?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Feb 2017 11:57:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Low-power-Timer-issue/m-p/628804#M307</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-02-17T11:57:08Z</dc:date>
    </item>
    <item>
      <title>Re: Low power Timer issue</title>
      <link>https://community.nxp.com/t5/S32K/Low-power-Timer-issue/m-p/628805#M308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Daniel:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks for your reply! this is caused I want to change to channel 2.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; According to your guide, the code is as below:&lt;/P&gt;&lt;P&gt;&amp;nbsp; void LPIT_ISR1(void)&lt;BR /&gt;&amp;nbsp; {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPIT_DRV_ClearInterruptFlagTimerChannels(FSL_LPIT1, (1 &amp;lt;&amp;lt;1));&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; GPIO_HAL_TogglePins(PTB,1&amp;lt;&amp;lt;5);&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; But it stil can't enter channel 1 interrupt function, even I closed channel 0 as below:&lt;/P&gt;&lt;P&gt;&amp;nbsp; //&amp;nbsp; INT_SYS_InstallHandler(48,&amp;amp;LPIT_ISR,(isr_t*)0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; INT_SYS_InstallHandler(49,&amp;amp;LPIT_ISR1,(isr_t*)0);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPIT_DRV_Init(FSL_LPIT1, &amp;amp;lpit1_InitConfig);&lt;BR /&gt;&amp;nbsp; //&amp;nbsp; LPIT_DRV_InitChannel(FSL_LPIT1, 0, &amp;amp;lpit1_ChnConfig0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPIT_DRV_InitChannel(FSL_LPIT1, 1, &amp;amp;lpit1_ChnConfig1);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; // LPIT_DRV_StartTimerChannels(FSL_LPIT1, (1 &amp;lt;&amp;lt; 0));&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPIT_DRV_StartTimerChannels(FSL_LPIT1, (1 &amp;lt;&amp;lt; 1));&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Can you help try in your board?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Feb 2017 01:15:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Low-power-Timer-issue/m-p/628805#M308</guid>
      <dc:creator>huaping</dc:creator>
      <dc:date>2017-02-20T01:15:30Z</dc:date>
    </item>
    <item>
      <title>Re: Low power Timer issue</title>
      <link>https://community.nxp.com/t5/S32K/Low-power-Timer-issue/m-p/628806#M309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have tried your code on two boards and it works on the new S32K144EVB-Q100 with N47T. But it doesn’t work on FRDMPK144-Q100 with N77P. I have rewritten the code without SDK, but it doesn’t work either. Although the flag is set, it won’t go into ISR. The problem is in the N77P mask set which is a prototype. &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 07:48:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Low-power-Timer-issue/m-p/628806#M309</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2017-02-22T07:48:32Z</dc:date>
    </item>
  </channel>
</rss>