<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: EEPROM Emulation on S32K12 Controller</title>
    <link>https://community.nxp.com/t5/S32K/EEPROM-Emulation-on-S32K12-Controller/m-p/1791926#M30886</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52613"&gt;@davidtosenovjan&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Looks like Fee driver is Autosar based. Is Fee is available without autosar??&lt;/P&gt;</description>
    <pubDate>Fri, 19 Jan 2024 12:35:59 GMT</pubDate>
    <dc:creator>Riyasma07</dc:creator>
    <dc:date>2024-01-19T12:35:59Z</dc:date>
    <item>
      <title>EEPROM Emulation on S32K12 Controller</title>
      <link>https://community.nxp.com/t5/S32K/EEPROM-Emulation-on-S32K12-Controller/m-p/1766152#M29169</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Rahul3_0-1701321145116.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/252220iF765D4BB5CD69C86/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Rahul3_0-1701321145116.png" alt="Rahul3_0-1701321145116.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Rahul3_0-1701321145116.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;i want to use to D flash memory of s32k312 controller as a EEPROM Emulation where i found this doc from NXP website which is s32k3 memory guide 3.2 Write or program section 2nd paragraph 4th line where i can see the statement like "When data Flash is used for EEPROM emulation, approved drivers by NXP can do an over programming in a 64 bit ECC segment, this allows to over-program the same location up to 3 times without performing an erase operation in the sector " could anyone explain it please more clearly because i want to use it as eeprom now where i want to write /read individual byte is this possible and how to use it (drivers/sdk )supported ? #S32K3 #EEPROM&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;rahul&lt;/P&gt;</description>
      <pubDate>Thu, 30 Nov 2023 05:19:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EEPROM-Emulation-on-S32K12-Controller/m-p/1766152#M29169</guid>
      <dc:creator>Rahul3</dc:creator>
      <dc:date>2023-11-30T05:19:22Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM Emulation on S32K12 Controller</title>
      <link>https://community.nxp.com/t5/S32K/EEPROM-Emulation-on-S32K12-Controller/m-p/1767418#M29245</link>
      <description>&lt;P&gt;On this device there EEPROM is emulated by SW in the data flash. For understanding the principle I could recommend following appnote (although written for different platform, the principle is the same): &lt;A href="https://www.nxp.com/docs/en/application-note/AN4868.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN4868.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Driver and example project you may find in S32DS, it is called Fee_Example_S32K3xx.&lt;/P&gt;
&lt;P&gt;In the installation directory, you may also find user manual for Flash EEPROM emulation driver:&lt;BR /&gt;c:\NXP\S32DS.3.4\S32DS\software\PlatformSDK_S32K3_2021_10\SW32K3_RTD_4_4_1_0_0_D2110\Fee_TS_T40D34M10I0R0\doc\&lt;/P&gt;
&lt;P&gt;I would strongly recommend to use our driver.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Dec 2023 17:13:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EEPROM-Emulation-on-S32K12-Controller/m-p/1767418#M29245</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-12-01T17:13:13Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM Emulation on S32K12 Controller</title>
      <link>https://community.nxp.com/t5/S32K/EEPROM-Emulation-on-S32K12-Controller/m-p/1791926#M30886</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52613"&gt;@davidtosenovjan&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Looks like Fee driver is Autosar based. Is Fee is available without autosar??&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jan 2024 12:35:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/EEPROM-Emulation-on-S32K12-Controller/m-p/1791926#M30886</guid>
      <dc:creator>Riyasma07</dc:creator>
      <dc:date>2024-01-19T12:35:59Z</dc:date>
    </item>
  </channel>
</rss>