<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ConfigTool Pins Tool does not set GPIO outputs in S32K</title>
    <link>https://community.nxp.com/t5/S32K/ConfigTool-Pins-Tool-does-not-set-GPIO-outputs/m-p/1791014#M30817</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I encounter an issue with pin configuration at S32. I am testing some features of S32K344 without using Autosar (non-autosar). SDK (RTD) version is 3.0.0.&lt;/P&gt;&lt;P&gt;I noticed that Pins Tool in Configuration Tool (CT) is generating GPIO outputs as disabled as seen at below. Other outputs, such as CAN Tx are OK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Due to this, initializing pins with below line is not set these GPIO pins as output.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);&lt;/LI-CODE&gt;&lt;P&gt;I need to config selected pin as output.&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Siul2_Port_Ip_SetOutputBuffer(PORTE_H_HALF, 1,	TRUE, PORT_MUX_AS_GPIO);		// set CAN4 STB E17&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I manually change code in "Siul2_Port_Ip_Cfg" but it is re-updated when I changed something in CT.&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is only one board configuration so it is not mixed or re-used.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this normal or am I missing something?&lt;/P&gt;&lt;P&gt;What Pins Tool&amp;nbsp;does if I need to configure all GPIOs as input or output?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2024-01-18 131543.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/258801i8A546E0547DFB9DA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot 2024-01-18 131543.png" alt="Screenshot 2024-01-18 131543.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 18 Jan 2024 10:32:50 GMT</pubDate>
    <dc:creator>anakha</dc:creator>
    <dc:date>2024-01-18T10:32:50Z</dc:date>
    <item>
      <title>ConfigTool Pins Tool does not set GPIO outputs</title>
      <link>https://community.nxp.com/t5/S32K/ConfigTool-Pins-Tool-does-not-set-GPIO-outputs/m-p/1791014#M30817</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I encounter an issue with pin configuration at S32. I am testing some features of S32K344 without using Autosar (non-autosar). SDK (RTD) version is 3.0.0.&lt;/P&gt;&lt;P&gt;I noticed that Pins Tool in Configuration Tool (CT) is generating GPIO outputs as disabled as seen at below. Other outputs, such as CAN Tx are OK.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Due to this, initializing pins with below line is not set these GPIO pins as output.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);&lt;/LI-CODE&gt;&lt;P&gt;I need to config selected pin as output.&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Siul2_Port_Ip_SetOutputBuffer(PORTE_H_HALF, 1,	TRUE, PORT_MUX_AS_GPIO);		// set CAN4 STB E17&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I manually change code in "Siul2_Port_Ip_Cfg" but it is re-updated when I changed something in CT.&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is only one board configuration so it is not mixed or re-used.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this normal or am I missing something?&lt;/P&gt;&lt;P&gt;What Pins Tool&amp;nbsp;does if I need to configure all GPIOs as input or output?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot 2024-01-18 131543.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/258801i8A546E0547DFB9DA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Screenshot 2024-01-18 131543.png" alt="Screenshot 2024-01-18 131543.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jan 2024 10:32:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ConfigTool-Pins-Tool-does-not-set-GPIO-outputs/m-p/1791014#M30817</guid>
      <dc:creator>anakha</dc:creator>
      <dc:date>2024-01-18T10:32:50Z</dc:date>
    </item>
    <item>
      <title>Re: ConfigTool Pins Tool does not set GPIO outputs</title>
      <link>https://community.nxp.com/t5/S32K/ConfigTool-Pins-Tool-does-not-set-GPIO-outputs/m-p/1791747#M30864</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/222923"&gt;@anakha&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Did you add any PowerAndGround or other pins that are routed by default to the project?&lt;/P&gt;
&lt;P&gt;If so, can you remove it? There is no point in adding these pins.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 19 Jan 2024 08:46:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ConfigTool-Pins-Tool-does-not-set-GPIO-outputs/m-p/1791747#M30864</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-01-19T08:46:38Z</dc:date>
    </item>
    <item>
      <title>Re: ConfigTool Pins Tool does not set GPIO outputs</title>
      <link>https://community.nxp.com/t5/S32K/ConfigTool-Pins-Tool-does-not-set-GPIO-outputs/m-p/1791763#M30868</link>
      <description>That's works, thanks a lot</description>
      <pubDate>Fri, 19 Jan 2024 09:00:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ConfigTool-Pins-Tool-does-not-set-GPIO-outputs/m-p/1791763#M30868</guid>
      <dc:creator>anakha</dc:creator>
      <dc:date>2024-01-19T09:00:06Z</dc:date>
    </item>
  </channel>
</rss>