<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ISR latency in S32K</title>
    <link>https://community.nxp.com/t5/S32K/ISR-latency/m-p/1788514#M30639</link>
    <description>&lt;P&gt;Hi support,&lt;/P&gt;&lt;P&gt;Is there some data about the ISR latency of S32K3 serials.&lt;/P&gt;&lt;P&gt;I do a test on S32K324 used emios SAIC mode to capture edge. In the ISR, I flip a gpio.&lt;/P&gt;&lt;P&gt;The latency between the input signal and the flip signal is about 300ns, it seems to long for system clock 160MHz.&lt;/P&gt;&lt;P&gt;The priority of the interrupt is 1, the highest. And when I turn on CAN interrupt to send data which priority is 6. The latency is fluctuant, 300~600ns. It seems CAN interrupt&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 15 Jan 2024 06:15:39 GMT</pubDate>
    <dc:creator>ZhouPengfei</dc:creator>
    <dc:date>2024-01-15T06:15:39Z</dc:date>
    <item>
      <title>ISR latency</title>
      <link>https://community.nxp.com/t5/S32K/ISR-latency/m-p/1788514#M30639</link>
      <description>&lt;P&gt;Hi support,&lt;/P&gt;&lt;P&gt;Is there some data about the ISR latency of S32K3 serials.&lt;/P&gt;&lt;P&gt;I do a test on S32K324 used emios SAIC mode to capture edge. In the ISR, I flip a gpio.&lt;/P&gt;&lt;P&gt;The latency between the input signal and the flip signal is about 300ns, it seems to long for system clock 160MHz.&lt;/P&gt;&lt;P&gt;The priority of the interrupt is 1, the highest. And when I turn on CAN interrupt to send data which priority is 6. The latency is fluctuant, 300~600ns. It seems CAN interrupt&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jan 2024 06:15:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ISR-latency/m-p/1788514#M30639</guid>
      <dc:creator>ZhouPengfei</dc:creator>
      <dc:date>2024-01-15T06:15:39Z</dc:date>
    </item>
    <item>
      <title>Re: ISR latency</title>
      <link>https://community.nxp.com/t5/S32K/ISR-latency/m-p/1788982#M30669</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224018"&gt;@ZhouPengfei&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;ISR latency depends on various factors. You can find a list of these factors and how to measure interrupt latency in this application note:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12078.pdf" target="_blank"&gt;Measuring Interrupt Latency&lt;/A&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;This application note describes how to measure the interrupt latency of the i.MX RT1050 device, but the steps to measure and factors to take into account are the same. I hope you find this helpful.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Julián&lt;/P&gt;</description>
      <pubDate>Mon, 15 Jan 2024 21:56:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ISR-latency/m-p/1788982#M30669</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2024-01-15T21:56:40Z</dc:date>
    </item>
  </channel>
</rss>