<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: s32k144 uart flow control in S32K</title>
    <link>https://community.nxp.com/t5/S32K/s32k144-uart-flow-control/m-p/817983#M3063</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andrew,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hardware flow control support for the request to send (RTS) and clear to send (CTS) signals.&lt;/P&gt;&lt;P&gt;The corresponding pins should be configured&amp;nbsp;by pin mux as LPUART RTS/CTS.&lt;/P&gt;&lt;P&gt;The alternatives for each pin you can find in the pinout in the S32K144_IO_Signal _Description_Input_Multiplexing.xlsx&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the configuration&amp;nbsp;of RTS or CTS look at the chapter&amp;nbsp;51.3.1.11 LPUART Modem IrDA Register (MODIR)&lt;/P&gt;&lt;P&gt;Related chapter 51.4.2.2 Hardware flow control&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 Aug 2018 08:00:11 GMT</pubDate>
    <dc:creator>dianabatrlova</dc:creator>
    <dc:date>2018-08-27T08:00:11Z</dc:date>
    <item>
      <title>s32k144 uart flow control</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-uart-flow-control/m-p/817982#M3062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working with the S32k144 development board, and I would like to use lpuart1&amp;nbsp;for communication. Since the messages are large, I need full hardware flow control support.&amp;nbsp;Does anyone know how to enable hardware flow control support on lpuart1?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Aug 2018 17:07:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-uart-flow-control/m-p/817982#M3062</guid>
      <dc:creator>ainwood</dc:creator>
      <dc:date>2018-08-22T17:07:16Z</dc:date>
    </item>
    <item>
      <title>Re: s32k144 uart flow control</title>
      <link>https://community.nxp.com/t5/S32K/s32k144-uart-flow-control/m-p/817983#M3063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andrew,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hardware flow control support for the request to send (RTS) and clear to send (CTS) signals.&lt;/P&gt;&lt;P&gt;The corresponding pins should be configured&amp;nbsp;by pin mux as LPUART RTS/CTS.&lt;/P&gt;&lt;P&gt;The alternatives for each pin you can find in the pinout in the S32K144_IO_Signal _Description_Input_Multiplexing.xlsx&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the configuration&amp;nbsp;of RTS or CTS look at the chapter&amp;nbsp;51.3.1.11 LPUART Modem IrDA Register (MODIR)&lt;/P&gt;&lt;P&gt;Related chapter 51.4.2.2 Hardware flow control&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Diana&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Aug 2018 08:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k144-uart-flow-control/m-p/817983#M3063</guid>
      <dc:creator>dianabatrlova</dc:creator>
      <dc:date>2018-08-27T08:00:11Z</dc:date>
    </item>
  </channel>
</rss>