<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックExecution from RAM - S32K</title>
    <link>https://community.nxp.com/t5/S32K/Execution-from-RAM-S32K/m-p/817526#M3048</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, i have been trying out the Keil&amp;nbsp; MDK Blinky Example given in the S32K SDK using the &lt;STRONG&gt;S32K144 EVB&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;C:\Keil_v5\ARM\PACK\Keil\S32_SDK_DFP\1.2.0\addon_mdk\Boards\NXP\S32K144-EVB\RTX5_Blinky&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i set the project configuration to use Flash i.e. execute from Flash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65666iE777950406B46D77/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The application runs flawlessly. However when i set it to RAM, build it and try to load it to the device, it gives the following error.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65667iC7AF5448887CDFA3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As it can be seen from the error the location its referring to is RAM, so obviously it is not going to work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have my settings configured as below using the CMSIS-DAP Debugger&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65668i77032627DB64CFC0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_7.png" alt="pastedImage_7.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65669i206327EDEE988146/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_8.png" alt="pastedImage_8.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The same issue occurs when i plug the ULINK2 to the on-board JTAG/SWD header J14 and try programming via ULINK.&lt;/P&gt;&lt;P&gt;Has anyone experienced this issue ? Any suggestions ? I plan to use the Keil MDK toolchain for all development.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Jul 2018 11:43:03 GMT</pubDate>
    <dc:creator>testbed</dc:creator>
    <dc:date>2018-07-17T11:43:03Z</dc:date>
    <item>
      <title>Execution from RAM - S32K</title>
      <link>https://community.nxp.com/t5/S32K/Execution-from-RAM-S32K/m-p/817526#M3048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, i have been trying out the Keil&amp;nbsp; MDK Blinky Example given in the S32K SDK using the &lt;STRONG&gt;S32K144 EVB&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;C:\Keil_v5\ARM\PACK\Keil\S32_SDK_DFP\1.2.0\addon_mdk\Boards\NXP\S32K144-EVB\RTX5_Blinky&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i set the project configuration to use Flash i.e. execute from Flash&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65666iE777950406B46D77/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The application runs flawlessly. However when i set it to RAM, build it and try to load it to the device, it gives the following error.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65667iC7AF5448887CDFA3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;As it can be seen from the error the location its referring to is RAM, so obviously it is not going to work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have my settings configured as below using the CMSIS-DAP Debugger&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65668i77032627DB64CFC0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_7.png" alt="pastedImage_7.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/65669i206327EDEE988146/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_8.png" alt="pastedImage_8.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The same issue occurs when i plug the ULINK2 to the on-board JTAG/SWD header J14 and try programming via ULINK.&lt;/P&gt;&lt;P&gt;Has anyone experienced this issue ? Any suggestions ? I plan to use the Keil MDK toolchain for all development.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Jul 2018 11:43:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Execution-from-RAM-S32K/m-p/817526#M3048</guid>
      <dc:creator>testbed</dc:creator>
      <dc:date>2018-07-17T11:43:03Z</dc:date>
    </item>
  </channel>
</rss>