<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K344 MCU LPUART configuration issue</title>
    <link>https://community.nxp.com/t5/S32K/S32K344-MCU-LPUART-configuration-issue/m-p/1783876#M30297</link>
    <description>&lt;P&gt;Hi Team&lt;/P&gt;&lt;P&gt;I am working on one of the projects that usea S32K344 MCU. In that i am facing UART working problem in which i am not able to communicate via UART. Can you please provide solution for this or uart example code ?&lt;BR /&gt;&lt;BR /&gt;Platform i am using is S32 Design Studio v3.5(Ubuntu 20.04 LTS).&lt;/P&gt;&lt;P&gt;Project : RTD AUTOSAR 4.4&lt;BR /&gt;* Platform : CORTEXM&lt;BR /&gt;* Autosar Version : 4.4.0&lt;BR /&gt;* Autosar Revision : ASR_REL_4_4_REV_0000&lt;BR /&gt;* SW Version : 1.0.0&lt;BR /&gt;* Build Version : S32K3_RTD_1_0_0_D2110_ASR_REL_4_4_REV_0000_20211007&lt;/P&gt;&lt;P&gt;************************************************************************************************************&lt;/P&gt;</description>
    <pubDate>Sat, 06 Jan 2024 11:14:30 GMT</pubDate>
    <dc:creator>nitish2</dc:creator>
    <dc:date>2024-01-06T11:14:30Z</dc:date>
    <item>
      <title>S32K344 MCU LPUART configuration issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-MCU-LPUART-configuration-issue/m-p/1783876#M30297</link>
      <description>&lt;P&gt;Hi Team&lt;/P&gt;&lt;P&gt;I am working on one of the projects that usea S32K344 MCU. In that i am facing UART working problem in which i am not able to communicate via UART. Can you please provide solution for this or uart example code ?&lt;BR /&gt;&lt;BR /&gt;Platform i am using is S32 Design Studio v3.5(Ubuntu 20.04 LTS).&lt;/P&gt;&lt;P&gt;Project : RTD AUTOSAR 4.4&lt;BR /&gt;* Platform : CORTEXM&lt;BR /&gt;* Autosar Version : 4.4.0&lt;BR /&gt;* Autosar Revision : ASR_REL_4_4_REV_0000&lt;BR /&gt;* SW Version : 1.0.0&lt;BR /&gt;* Build Version : S32K3_RTD_1_0_0_D2110_ASR_REL_4_4_REV_0000_20211007&lt;/P&gt;&lt;P&gt;************************************************************************************************************&lt;/P&gt;</description>
      <pubDate>Sat, 06 Jan 2024 11:14:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-MCU-LPUART-configuration-issue/m-p/1783876#M30297</guid>
      <dc:creator>nitish2</dc:creator>
      <dc:date>2024-01-06T11:14:30Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MCU LPUART configuration issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-MCU-LPUART-configuration-issue/m-p/1783877#M30298</link>
      <description>&lt;P&gt;hi team&lt;BR /&gt;I am attaching the &lt;EM&gt;S32K344.mex&lt;/EM&gt; file for the reference in which &lt;EM&gt;LPUART&lt;/EM&gt; configs. can be found.&lt;/P&gt;</description>
      <pubDate>Sat, 06 Jan 2024 11:17:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-MCU-LPUART-configuration-issue/m-p/1783877#M30298</guid>
      <dc:creator>nitish2</dc:creator>
      <dc:date>2024-01-06T11:17:23Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MCU LPUART configuration issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-MCU-LPUART-configuration-issue/m-p/1786792#M30501</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;I don't know the specific situation of S32DS v3.5 in Ubuntu, because I have only used Windows.&lt;BR /&gt;As far as I know, S32K3 RTD 1.0.0 was released 3 years ago. Logically speaking, and the current S32DS v3.5 should be S32K3 RTD 4.0.x.&lt;BR /&gt;Will you see examples of S32K3 RTD after&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;FONT color="#0000FF"&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32DS-Extensions-Updates-Explanation-and-How-To-Use/ta-p/1128543" target="_self"&gt;Online Package Installation&lt;/A&gt;&lt;/FONT&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;it on your S32DS v3.5?&lt;BR /&gt;File -&amp;gt; New -&amp;gt; S32DS Project from Example&lt;BR /&gt;LpuartFlexio_Uart_Ip_Example and Uart_Example.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jan 2024 04:37:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-MCU-LPUART-configuration-issue/m-p/1786792#M30501</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2024-01-11T04:37:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32K344 MCU LPUART configuration issue</title>
      <link>https://community.nxp.com/t5/S32K/S32K344-MCU-LPUART-configuration-issue/m-p/1788355#M30630</link>
      <description>&lt;P&gt;Hi&lt;BR /&gt;I tried over windows laptop for UART issue. In windows i could open and configure .mex file for UART. Don't know why in ubuntu laptop i could not do the same.&lt;/P&gt;</description>
      <pubDate>Sun, 14 Jan 2024 10:04:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K344-MCU-LPUART-configuration-issue/m-p/1788355#M30630</guid>
      <dc:creator>nitish2</dc:creator>
      <dc:date>2024-01-14T10:04:44Z</dc:date>
    </item>
  </channel>
</rss>