<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックCannot enter pin configuration for S32K338</title>
    <link>https://community.nxp.com/t5/S32K/Cannot-enter-pin-configuration-for-S32K338/m-p/1782530#M30180</link>
    <description>&lt;P&gt;I am trying to simply enter the pin configuration tool for the S32K338 SOC. When creating a project, I can select the specific part number and package, but when I try to enter the Pin Configuration tool, I see an error that others have seen elsewhere stating &lt;STRONG&gt;MCU is Not Selected.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;This is (to my knowledge) because the Project is blank. However, when I click the Project drop down and select my newly created project with the K338, a new error window pops open stating&lt;STRONG&gt; 'Opening the configuration failed due to an unknown reason.'&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;This error appears for any and all proejcts, even the Project_Pins_and_Clock_Training training project I've downloaded that has all files included.&lt;/P&gt;&lt;P&gt;I'm running S32DS 3.5.8 with what I think is everything needed to do this installed. I did however see that there is no SDK available to select when I first created the project...&lt;/P&gt;</description>
    <pubDate>Wed, 03 Jan 2024 23:38:30 GMT</pubDate>
    <dc:creator>AW88</dc:creator>
    <dc:date>2024-01-03T23:38:30Z</dc:date>
    <item>
      <title>Cannot enter pin configuration for S32K338</title>
      <link>https://community.nxp.com/t5/S32K/Cannot-enter-pin-configuration-for-S32K338/m-p/1782530#M30180</link>
      <description>&lt;P&gt;I am trying to simply enter the pin configuration tool for the S32K338 SOC. When creating a project, I can select the specific part number and package, but when I try to enter the Pin Configuration tool, I see an error that others have seen elsewhere stating &lt;STRONG&gt;MCU is Not Selected.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;This is (to my knowledge) because the Project is blank. However, when I click the Project drop down and select my newly created project with the K338, a new error window pops open stating&lt;STRONG&gt; 'Opening the configuration failed due to an unknown reason.'&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;This error appears for any and all proejcts, even the Project_Pins_and_Clock_Training training project I've downloaded that has all files included.&lt;/P&gt;&lt;P&gt;I'm running S32DS 3.5.8 with what I think is everything needed to do this installed. I did however see that there is no SDK available to select when I first created the project...&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jan 2024 23:38:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Cannot-enter-pin-configuration-for-S32K338/m-p/1782530#M30180</guid>
      <dc:creator>AW88</dc:creator>
      <dc:date>2024-01-03T23:38:30Z</dc:date>
    </item>
  </channel>
</rss>