<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: S32K EEPROM CONFIGURATION in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K-EEPROM-CONFIGURATION/m-p/1781221#M30067</link>
    <description>&lt;P&gt;It is needed to perform program partition command once (for blank new device or with performed mass erase operation). There is an example code in S32DS (flash_partitioning_s32k1..).&lt;/P&gt;
&lt;P&gt;For any other use, it is needed to perform flash_partitioning operation according user configuration. Pay attention to AN11983 - Using the S32K1xx EEPROM Functionality:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11983.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN11983.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;EEPROM portion of FlexNVM will be accesses over FlexRAM memory address space.&lt;BR /&gt;Data flash portion of FlexNVM will be accesses ordinary way i.e. reading of flash address directly and erasing/programming of flash address.&lt;/P&gt;
&lt;P&gt;Regarding mass erase, pay attention here:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/data-flash-partition/m-p/1073360" target="_blank"&gt;https://community.nxp.com/t5/S32K/data-flash-partition/m-p/1073360&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 29 Dec 2023 13:59:17 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2023-12-29T13:59:17Z</dc:date>
    <item>
      <title>S32K EEPROM CONFIGURATION</title>
      <link>https://community.nxp.com/t5/S32K/S32K-EEPROM-CONFIGURATION/m-p/1780288#M29962</link>
      <description>&lt;P&gt;1. How to mass erase to restore the partition of flash to configure 2KB flexRAM as EEPROM.&lt;BR /&gt;2.Share the example which have following features.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;- EEE image loaded into RAM,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; - Records read directly from RAM. No EEE operation.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;- Records written directly to RAM. Image automatically synchronized with EEE flash.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Dec 2023 05:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-EEPROM-CONFIGURATION/m-p/1780288#M29962</guid>
      <dc:creator>SivaB</dc:creator>
      <dc:date>2023-12-27T05:58:45Z</dc:date>
    </item>
    <item>
      <title>Re: S32K EEPROM CONFIGURATION</title>
      <link>https://community.nxp.com/t5/S32K/S32K-EEPROM-CONFIGURATION/m-p/1781221#M30067</link>
      <description>&lt;P&gt;It is needed to perform program partition command once (for blank new device or with performed mass erase operation). There is an example code in S32DS (flash_partitioning_s32k1..).&lt;/P&gt;
&lt;P&gt;For any other use, it is needed to perform flash_partitioning operation according user configuration. Pay attention to AN11983 - Using the S32K1xx EEPROM Functionality:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11983.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN11983.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;EEPROM portion of FlexNVM will be accesses over FlexRAM memory address space.&lt;BR /&gt;Data flash portion of FlexNVM will be accesses ordinary way i.e. reading of flash address directly and erasing/programming of flash address.&lt;/P&gt;
&lt;P&gt;Regarding mass erase, pay attention here:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/S32K/data-flash-partition/m-p/1073360" target="_blank"&gt;https://community.nxp.com/t5/S32K/data-flash-partition/m-p/1073360&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Dec 2023 13:59:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-EEPROM-CONFIGURATION/m-p/1781221#M30067</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2023-12-29T13:59:17Z</dc:date>
    </item>
  </channel>
</rss>