<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックLow Power Mode on S32K344</title>
    <link>https://community.nxp.com/t5/S32K/Low-Power-Mode-on-S32K344/m-p/1780943#M30032</link>
    <description>&lt;P&gt;From the reference manual and the application note I understand that the MCU resets(even if we use the wakeup unit to exit) everytime we exit Standby mode and enter RUN mode. I have a big project that runs multiple peripherals all the time. But I want to have SLEEP mode where I make the MCU to go to sleep(low power mode) and start execution from where I last stopped. But my RAM contents are lost due to the reset on standby exit and my program counter starts from main.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any provision to have this functionality that I have described without losing my RAM contents.&lt;/P&gt;</description>
    <pubDate>Thu, 28 Dec 2023 15:51:59 GMT</pubDate>
    <dc:creator>enthuCutlet</dc:creator>
    <dc:date>2023-12-28T15:51:59Z</dc:date>
    <item>
      <title>Low Power Mode on S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Low-Power-Mode-on-S32K344/m-p/1780943#M30032</link>
      <description>&lt;P&gt;From the reference manual and the application note I understand that the MCU resets(even if we use the wakeup unit to exit) everytime we exit Standby mode and enter RUN mode. I have a big project that runs multiple peripherals all the time. But I want to have SLEEP mode where I make the MCU to go to sleep(low power mode) and start execution from where I last stopped. But my RAM contents are lost due to the reset on standby exit and my program counter starts from main.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any provision to have this functionality that I have described without losing my RAM contents.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Dec 2023 15:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Low-Power-Mode-on-S32K344/m-p/1780943#M30032</guid>
      <dc:creator>enthuCutlet</dc:creator>
      <dc:date>2023-12-28T15:51:59Z</dc:date>
    </item>
    <item>
      <title>Re: Low Power Mode on S32K344</title>
      <link>https://community.nxp.com/t5/S32K/Low-Power-Mode-on-S32K344/m-p/1781380#M30083</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@enthuCutlet" target="_blank"&gt;Hi@enthuCutlet&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;S32k344 have 32KB Standby RAM space which can be used to save data and the data won't be lost even wake-up from standby mode.&lt;/P&gt;
&lt;P&gt;Here is some demo and application note for you to better understand Standby RAM .&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Low-Power-Management-AN-and-demos/ta-p/1527724" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-Low-Power-Management-AN-and-demos/ta-p/1527724&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;you can take a look at the demo "&lt;FONT size="2"&gt;&lt;STRONG&gt;S32K344_RTC_StandbyRAM_Wkup_S32DS_3_4_RTD_LLD_2_0.ZIP&lt;/STRONG&gt;&lt;/FONT&gt;"&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jan 2024 02:39:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Low-Power-Mode-on-S32K344/m-p/1781380#M30083</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2024-01-02T02:39:13Z</dc:date>
    </item>
  </channel>
</rss>