<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: SPD demo BIST config question</title>
    <link>https://community.nxp.com/t5/S32K/SPD-demo-BIST-config-question/m-p/1780835#M30019</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;1. Is this a design flaw or do users need to manually modify certain code?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Well, this would be the question to designers of the SW. But for sure if you want run the PLL for BIST, you need to set those bits.&lt;/P&gt;
&lt;P&gt;If you like the feedback from SW owners, please submit a ticket at NXP.com so it will reach them.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
    <pubDate>Thu, 28 Dec 2023 08:37:02 GMT</pubDate>
    <dc:creator>petervlna</dc:creator>
    <dc:date>2023-12-28T08:37:02Z</dc:date>
    <item>
      <title>SPD demo BIST config question</title>
      <link>https://community.nxp.com/t5/S32K/SPD-demo-BIST-config-question/m-p/1779162#M29896</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;Pre-Information:&lt;BR /&gt;In the "safety-&amp;gt;STCU2" section of S32K3XXRM, there is a register related to PLL monitoring located at STCU2-&amp;gt;RUNSW. According to the description, when our clock configuration uses PLL, we need to enable these two fields.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pusoy_1-1703235115735.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255648i174F0EA7EF80E9DB/image-size/large?v=v2&amp;amp;px=999" role="button" title="Pusoy_1-1703235115735.png" alt="Pusoy_1-1703235115735.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Pusoy_1-1703235115735.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In the demo provided by &lt;FONT size="4"&gt;S32K3 Safety Peripheral Drivers version 1.0.3&amp;nbsp;&lt;/FONT&gt;&lt;A href="https://nxp.flexnetoperations.com/control/frse/download?element=14273477" target="_blank" rel="nofollow noopener noreferrer"&gt;Design : Product Download : Files (flexnetoperations.com)&lt;/A&gt;, PLL is enabled.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pusoy_0-1703235078210.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255647iA4A3ACB7E527C36B/image-size/large?v=v2&amp;amp;px=999" role="button" title="Pusoy_0-1703235078210.png" alt="Pusoy_0-1703235078210.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Pusoy_0-1703235078210.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Based on the above information, these two bits should be set to 1 in the STCU2-&amp;gt;RUNSW register in the demo.&lt;BR /&gt;And in the main.c file of the provided demo, the place where this register is set is in BIST_RUN()-&amp;gt;Bist_Specific_Run()-&amp;gt;Bist_SelfTestTrigger()-&amp;gt;SAFETYBASE_REG_WRITE32(BIST_STCU_RUNSW_REG, BIST_STCU_RUNSW_RUN_BIT);&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pusoy_2-1703235253849.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255650i91A39BA4078CA2B3/image-size/large?v=v2&amp;amp;px=999" role="button" title="Pusoy_2-1703235253849.png" alt="Pusoy_2-1703235253849.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Pusoy_2-1703235253849.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, in the case where PLL is enabled in the clock configuration, the library driver provided by SPD does not set these two bits to 1.&lt;BR /&gt;&lt;BR /&gt;1. Is this a design flaw or do users need to manually modify certain code?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Dec 2023 08:58:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPD-demo-BIST-config-question/m-p/1779162#M29896</guid>
      <dc:creator>Pusoy</dc:creator>
      <dc:date>2023-12-22T08:58:44Z</dc:date>
    </item>
    <item>
      <title>Re: SPD demo BIST config question</title>
      <link>https://community.nxp.com/t5/S32K/SPD-demo-BIST-config-question/m-p/1780835#M30019</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;1. Is this a design flaw or do users need to manually modify certain code?&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;Well, this would be the question to designers of the SW. But for sure if you want run the PLL for BIST, you need to set those bits.&lt;/P&gt;
&lt;P&gt;If you like the feedback from SW owners, please submit a ticket at NXP.com so it will reach them.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Peter&lt;/P&gt;</description>
      <pubDate>Thu, 28 Dec 2023 08:37:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPD-demo-BIST-config-question/m-p/1780835#M30019</guid>
      <dc:creator>petervlna</dc:creator>
      <dc:date>2023-12-28T08:37:02Z</dc:date>
    </item>
  </channel>
</rss>