<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [S32K] Flash memory setting in VLPR Mode in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32K-Flash-memory-setting-in-VLPR-Mode/m-p/815055#M3001</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;There is no need to disable the FTFC module before entering VLPR. The VLPR clock configuration must be done before the transition.&lt;BR /&gt;In VLPR, no FTFC commands of any type are available and the Flash clock is restricted to 1MHz or less.&lt;BR /&gt;The Flash clock can be monitored externally at a CLKOUT pin. Please see Figure 27-1 RM rev.9&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76423iE62C50A9FDE2E430/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Oct 2018 10:11:00 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-10-22T10:11:00Z</dc:date>
    <item>
      <title>[S32K] Flash memory setting in VLPR Mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K-Flash-memory-setting-in-VLPR-Mode/m-p/815054#M3000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The reference manual of S32K mentions that it is necessary to disable the flash module before turning off FTFC clock prior to entering VLPR mode.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There is no flash driver de-initialize code available in S32 Design Studio. So, what is the right sequence to disable the flash module?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Also, how to verify that FLASH_CLK is already less than or equal to 1MHz?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Jing Yin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2018 06:12:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-Flash-memory-setting-in-VLPR-Mode/m-p/815054#M3000</guid>
      <dc:creator>jingyinwong</dc:creator>
      <dc:date>2018-10-22T06:12:08Z</dc:date>
    </item>
    <item>
      <title>Re: [S32K] Flash memory setting in VLPR Mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K-Flash-memory-setting-in-VLPR-Mode/m-p/815055#M3001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;There is no need to disable the FTFC module before entering VLPR. The VLPR clock configuration must be done before the transition.&lt;BR /&gt;In VLPR, no FTFC commands of any type are available and the Flash clock is restricted to 1MHz or less.&lt;BR /&gt;The Flash clock can be monitored externally at a CLKOUT pin. Please see Figure 27-1 RM rev.9&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76423iE62C50A9FDE2E430/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2018 10:11:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K-Flash-memory-setting-in-VLPR-Mode/m-p/815055#M3001</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-10-22T10:11:00Z</dc:date>
    </item>
  </channel>
</rss>