<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: S32K144 SPI Slave Mode Example</title>
    <link>https://community.nxp.com/t5/S32K/S32K144-SPI-Slave-Mode-Example/m-p/814666#M2999</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;There is LPSPI_transfer_S32K144 SDK example in S32DS.&lt;BR /&gt;The example uses two on board instances of LPSPI, one master and one slave. &lt;BR /&gt;The slave sends ADC results to the master.&lt;BR /&gt;Unfortunately, there is no non-SDK SPI slave example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Jun 2018 12:27:18 GMT</pubDate>
    <dc:creator>danielmartynek</dc:creator>
    <dc:date>2018-06-27T12:27:18Z</dc:date>
    <item>
      <title>S32K144 SPI Slave Mode Example</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-SPI-Slave-Mode-Example/m-p/814665#M2998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anyone provide an example code for the SPI slave mode? The Design Studio only has code for Master mode configuration. I have trouble in setting the configuration registers and also the interrupt.&lt;/P&gt;&lt;P&gt;I am trying to use an external master to acquire information from the S32K144. The master device will manage the clock and chip select.&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Jun 2018 17:48:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-SPI-Slave-Mode-Example/m-p/814665#M2998</guid>
      <dc:creator>chenguangjiang</dc:creator>
      <dc:date>2018-06-25T17:48:08Z</dc:date>
    </item>
    <item>
      <title>Re: S32K144 SPI Slave Mode Example</title>
      <link>https://community.nxp.com/t5/S32K/S32K144-SPI-Slave-Mode-Example/m-p/814666#M2999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;BR /&gt;There is LPSPI_transfer_S32K144 SDK example in S32DS.&lt;BR /&gt;The example uses two on board instances of LPSPI, one master and one slave. &lt;BR /&gt;The slave sends ADC results to the master.&lt;BR /&gt;Unfortunately, there is no non-SDK SPI slave example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jun 2018 12:27:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K144-SPI-Slave-Mode-Example/m-p/814666#M2999</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2018-06-27T12:27:18Z</dc:date>
    </item>
  </channel>
</rss>