<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Non Autosar Driver Example Code for S32k312 in S32K</title>
    <link>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1779955#M29935</link>
    <description>&lt;P&gt;Please offline install S32K3 RTD 2.0.x by refer to the discussion in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K3-Unified-Bootloader-Build-Issue/td-p/1653130" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K3-Unified-Bootloader-Build-Issue/td-p/1653130&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;After S32K3 RTD 2.0.x is correct installed. Import examples of S32K312, and then click on the "S32 Configuration Tool-&amp;gt;&lt;STRONG&gt;Update Code&lt;/STRONG&gt;" button.&lt;/P&gt;</description>
    <pubDate>Tue, 26 Dec 2023 08:20:38 GMT</pubDate>
    <dc:creator>Robin_Shen</dc:creator>
    <dc:date>2023-12-26T08:20:38Z</dc:date>
    <item>
      <title>Non Autosar Driver Example Code for S32k312</title>
      <link>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1778371#M29847</link>
      <description>&lt;P&gt;Hello Team,&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57959"&gt;@Robin_Shen&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm trying to find non Autosar driver code (Adc, Pwm, Spi, Can, I2c, Dio) for&amp;nbsp;Sk32k312. Please share if it is available with anyone.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Dev&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Dec 2023 05:37:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1778371#M29847</guid>
      <dc:creator>Dev15</dc:creator>
      <dc:date>2023-12-21T05:37:51Z</dc:date>
    </item>
    <item>
      <title>Re: Non Autosar Driver Example Code for S32k312</title>
      <link>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1778474#M29850</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN&gt;Dev,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Did you import it through File-&amp;gt;New-&amp;gt;S32DS Project from Example?&lt;BR /&gt;S32DS v3.5 + S32K3 RTD 3.0.x or 4.0.x does not have examples of S32K312EVB-Q172, only examples of S32K344, S32K358, and S32K396.&lt;BR /&gt;S32DS v3.4 + S32K3 RTD 2.0.x has examples of S32K312EVB-Q172.&lt;BR /&gt;It is recommended that you create a new S32K312 project and refer to the examples of S32K312 RTD 2.0.x or the examples of S32K344 RTD 3.0.x or 4.0.x.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Sorry for the inconvenience we bring you!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Thu, 21 Dec 2023 07:21:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1778474#M29850</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-12-21T07:21:57Z</dc:date>
    </item>
    <item>
      <title>Re: Non Autosar Driver Example Code for S32k312</title>
      <link>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1778514#M29853</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57959"&gt;@Robin_Shen&lt;/a&gt;&amp;nbsp;, Thank you very much for providing the details&lt;/P&gt;&lt;P&gt;Could you also please share me the details for S32K310 driver code&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;</description>
      <pubDate>Thu, 21 Dec 2023 07:57:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1778514#M29853</guid>
      <dc:creator>Dev15</dc:creator>
      <dc:date>2023-12-21T07:57:13Z</dc:date>
    </item>
    <item>
      <title>Re: Non Autosar Driver Example Code for S32k312</title>
      <link>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1778993#M29884</link>
      <description>&lt;P&gt;According to the release notes of S32K3 RTD 3.0.x and RTD 4.0.x, I saw that S32K310 is already in &lt;STRONG&gt;Supported Derivatives&lt;/STRONG&gt;. Unfortunately, there are currently no examples for S32K310. You need to create new project yourself and refer to examples of other chips.&lt;/P&gt;</description>
      <pubDate>Fri, 22 Dec 2023 04:17:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1778993#M29884</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-12-22T04:17:20Z</dc:date>
    </item>
    <item>
      <title>Re: Non Autosar Driver Example Code for S32k312</title>
      <link>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1779237#M29902</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57959"&gt;@Robin_Shen&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;I've installed following packages in S32 Design Studio v3.4 - SW32K3_S32DS_3.4.0_D2012.zip&amp;nbsp;&lt;/P&gt;&lt;P&gt;SW32K3_RTD_4.4_2.0.0_DS_updatesite_D2204.zip but I am not able to compile the example code for S32K312 controller. I even tried the S32 configuration tool for generating the code but the RTD is not generated. Mainly I need an non-Autosar based code for S32K312 evaluation board. Is it available? &amp;nbsp;Can you please give me proper procedure for compiling an non-Autosar based code.&lt;/P&gt;</description>
      <pubDate>Fri, 22 Dec 2023 11:04:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1779237#M29902</guid>
      <dc:creator>Dev15</dc:creator>
      <dc:date>2023-12-22T11:04:24Z</dc:date>
    </item>
    <item>
      <title>Re: Non Autosar Driver Example Code for S32k312</title>
      <link>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1779955#M29935</link>
      <description>&lt;P&gt;Please offline install S32K3 RTD 2.0.x by refer to the discussion in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K/S32K3-Unified-Bootloader-Build-Issue/td-p/1653130" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K3-Unified-Bootloader-Build-Issue/td-p/1653130&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;After S32K3 RTD 2.0.x is correct installed. Import examples of S32K312, and then click on the "S32 Configuration Tool-&amp;gt;&lt;STRONG&gt;Update Code&lt;/STRONG&gt;" button.&lt;/P&gt;</description>
      <pubDate>Tue, 26 Dec 2023 08:20:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1779955#M29935</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-12-26T08:20:38Z</dc:date>
    </item>
    <item>
      <title>Re: Non Autosar Driver Example Code for S32k312</title>
      <link>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1780332#M29966</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57959"&gt;@Robin_Shen&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I've tried the above-mentioned point but still the RTD is not generated. Am I still missing something? Can you please help? Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Dec 2023 06:56:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1780332#M29966</guid>
      <dc:creator>SandyHCL</dc:creator>
      <dc:date>2023-12-27T06:56:57Z</dc:date>
    </item>
    <item>
      <title>Re: Non Autosar Driver Example Code for S32k312</title>
      <link>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1780422#M29974</link>
      <description>&lt;P&gt;Please create a new question. Tell us the S32K3x part number\ version of IDE \ version of RTD, so that we can discuss it based on your specific situation.&lt;BR /&gt;I don't know which chip you are using. If it is S32K344, please refer to: &lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-offline-install-S32K3-RTD-3-0-0-in-S32DS-v3-5/ta-p/1753870" target="_self"&gt;HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Dec 2023 08:07:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/Non-Autosar-Driver-Example-Code-for-S32k312/m-p/1780422#M29974</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-12-27T08:07:53Z</dc:date>
    </item>
  </channel>
</rss>