<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic S32DS Using the keyword static to define a function or variable map cannot generate an address in S32K</title>
    <link>https://community.nxp.com/t5/S32K/S32DS-Using-the-keyword-static-to-define-a-function-or-variable/m-p/1779724#M29925</link>
    <description>&lt;P&gt;&lt;STRONG&gt;hello&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am using S32DS 3.5. 6; to develop S32K311.&lt;/P&gt;&lt;P&gt;I have defined a function using &lt;U&gt;&lt;STRONG&gt;static&lt;/STRONG&gt;&lt;/U&gt; keyword and after compilation, I can't find the address on the map file The function is defined in control_main. c file static void task3A(void)&lt;/P&gt;&lt;P&gt;debug:breakpoint to show the address bit of task3A 0x0040_13ac&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The function's address is not found in theMAP address range.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 25 Dec 2023 10:38:27 GMT</pubDate>
    <dc:creator>TM_207</dc:creator>
    <dc:date>2023-12-25T10:38:27Z</dc:date>
    <item>
      <title>S32DS Using the keyword static to define a function or variable map cannot generate an address</title>
      <link>https://community.nxp.com/t5/S32K/S32DS-Using-the-keyword-static-to-define-a-function-or-variable/m-p/1779724#M29925</link>
      <description>&lt;P&gt;&lt;STRONG&gt;hello&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am using S32DS 3.5. 6; to develop S32K311.&lt;/P&gt;&lt;P&gt;I have defined a function using &lt;U&gt;&lt;STRONG&gt;static&lt;/STRONG&gt;&lt;/U&gt; keyword and after compilation, I can't find the address on the map file The function is defined in control_main. c file static void task3A(void)&lt;/P&gt;&lt;P&gt;debug:breakpoint to show the address bit of task3A 0x0040_13ac&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The function's address is not found in theMAP address range.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Dec 2023 10:38:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32DS-Using-the-keyword-static-to-define-a-function-or-variable/m-p/1779724#M29925</guid>
      <dc:creator>TM_207</dc:creator>
      <dc:date>2023-12-25T10:38:27Z</dc:date>
    </item>
  </channel>
</rss>