<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックCAN receive error</title>
    <link>https://community.nxp.com/t5/S32K/CAN-receive-error/m-p/1779442#M29910</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;I have four can messages, but during reciving, the ID and data is not matched.&lt;BR /&gt;&lt;BR /&gt;transmit:&lt;BR /&gt;0xA1: 0x59, 0x00,0x08&lt;BR /&gt;0xA2: 0xB5&lt;BR /&gt;0xA3: 0xE1,0x00,0x08&lt;BR /&gt;0xA4: 0x22,0x80&lt;BR /&gt;&lt;BR /&gt;but I received the message in S32K144 are as below:&lt;BR /&gt;&lt;BR /&gt;0xA1: 0xB5&lt;BR /&gt;0xA3: 0x22,0x80&lt;BR /&gt;&lt;BR /&gt;The data and ID is not matched.&lt;BR /&gt;&lt;BR /&gt;What is the reason?&lt;/P&gt;</description>
    <pubDate>Sun, 24 Dec 2023 08:58:34 GMT</pubDate>
    <dc:creator>HanchunHarry</dc:creator>
    <dc:date>2023-12-24T08:58:34Z</dc:date>
    <item>
      <title>CAN receive error</title>
      <link>https://community.nxp.com/t5/S32K/CAN-receive-error/m-p/1779442#M29910</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;BR /&gt;I have four can messages, but during reciving, the ID and data is not matched.&lt;BR /&gt;&lt;BR /&gt;transmit:&lt;BR /&gt;0xA1: 0x59, 0x00,0x08&lt;BR /&gt;0xA2: 0xB5&lt;BR /&gt;0xA3: 0xE1,0x00,0x08&lt;BR /&gt;0xA4: 0x22,0x80&lt;BR /&gt;&lt;BR /&gt;but I received the message in S32K144 are as below:&lt;BR /&gt;&lt;BR /&gt;0xA1: 0xB5&lt;BR /&gt;0xA3: 0x22,0x80&lt;BR /&gt;&lt;BR /&gt;The data and ID is not matched.&lt;BR /&gt;&lt;BR /&gt;What is the reason?&lt;/P&gt;</description>
      <pubDate>Sun, 24 Dec 2023 08:58:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-receive-error/m-p/1779442#M29910</guid>
      <dc:creator>HanchunHarry</dc:creator>
      <dc:date>2023-12-24T08:58:34Z</dc:date>
    </item>
    <item>
      <title>Re: CAN receive error</title>
      <link>https://community.nxp.com/t5/S32K/CAN-receive-error/m-p/1780004#M29941</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@Hanchun" target="_blank"&gt;Hi@HanchunHarry&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;please refer to this article, these demo are all tested.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K1xx-FlexCAN-Mask-Setting-Demo/ta-p/1519753" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/S32K1xx-FlexCAN-Mask-Setting-Demo/ta-p/1519753&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Dec 2023 09:32:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/CAN-receive-error/m-p/1780004#M29941</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-12-26T09:32:15Z</dc:date>
    </item>
  </channel>
</rss>