<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K312 CAN not working Normal mode</title>
    <link>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1778812#M29870</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello, I'm using the tja1055 as a transceiver. I'm facilitating two-way communication (meaning there's a receiver and a transmitter). I'm using the s32k312 as the processor. As a trial, I have a test code for receiving and transmitting in loopback mode. When I test this code, it works seamlessly. However, in normal mode, I'm not receiving the 'Receive callback.' I can see the signal of the message I send on the RX pin of the receiver transceiver. My message-sending code is a modified version of my loopback code, and my receiver code is the same code with the sending part turned off&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 21 Dec 2023 15:59:19 GMT</pubDate>
    <dc:creator>rexoplans</dc:creator>
    <dc:date>2023-12-21T15:59:19Z</dc:date>
    <item>
      <title>S32K312 CAN not working Normal mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1778812#M29870</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, I'm using the tja1055 as a transceiver. I'm facilitating two-way communication (meaning there's a receiver and a transmitter). I'm using the s32k312 as the processor. As a trial, I have a test code for receiving and transmitting in loopback mode. When I test this code, it works seamlessly. However, in normal mode, I'm not receiving the 'Receive callback.' I can see the signal of the message I send on the RX pin of the receiver transceiver. My message-sending code is a modified version of my loopback code, and my receiver code is the same code with the sending part turned off&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Dec 2023 15:59:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1778812#M29870</guid>
      <dc:creator>rexoplans</dc:creator>
      <dc:date>2023-12-21T15:59:19Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 CAN not working Normal mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1778956#M29879</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@rexoplans" target="_blank"&gt;Hi@rexoplans&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;1.please double check wether TJA1055 is right configured before use.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1703211729939.png" style="width: 501px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255597i42D9A8F49CBDBCC0/image-dimensions/501x228?v=v2" width="501" height="228" role="button" title="Senlent_0-1703211729939.png" alt="Senlent_0-1703211729939.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Dec 2023 02:23:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1778956#M29879</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-12-22T02:23:59Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 CAN not working Normal mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779063#M29888</link>
      <description>Hello, I'm seeing VCC voltage when the line is idle (no messages are being sent). Doesn't this indicate that two transceivers are active and in normal mode? Also, I'm applying 1-1 values to the STB and EN pins. I'm seeing 12V on the INH pins of both transceivers (12 volts being my BAT voltage).</description>
      <pubDate>Fri, 22 Dec 2023 06:56:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779063#M29888</guid>
      <dc:creator>rexoplans</dc:creator>
      <dc:date>2023-12-22T06:56:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 CAN not working Normal mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779092#M29890</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@rexoplans" target="_blank"&gt;Hi@rexoplans&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;1. Have you configured and initialized the pins correctly?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_1-1703230292780.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255633iD5327634C203B2B5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Senlent_1-1703230292780.png" alt="Senlent_1-1703230292780.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;2. If everything is configured correctly, then you can use tools such as an oscilloscope or logic analyzer to test whether the TX output on the MCU side has the correct output.&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;3. If the TX on the MCU side is normal, then solve the problem of TJA1055. Usually the STB and EN pins should be controlled by the MCU side.&lt;/P&gt;
&lt;P&gt;Input requirements for STB and EN pins&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Senlent_0-1703229281514.png" style="width: 731px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255632i4C45DFABBBED5902/image-dimensions/731x178?v=v2" width="731" height="178" role="button" title="Senlent_0-1703229281514.png" alt="Senlent_0-1703229281514.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Dec 2023 07:36:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779092#M29890</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-12-22T07:36:48Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 CAN not working Normal mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779094#M29891</link>
      <description>Hello, my pin numbers are correct, but I'm not entirely sure about the pin configuration. Here's the situation: I'm observing output on the RX pin of the receiver card through the oscilloscope, and my signal appears correct. Shouldn't I not be seeing a signal if the transceivers weren't activated? My Tx pin configuration seems correct; I'll check on the configuration of my RX pin. In fact, I'll leave the configuration I've made below.</description>
      <pubDate>Fri, 22 Dec 2023 07:42:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779094#M29891</guid>
      <dc:creator>rexoplans</dc:creator>
      <dc:date>2023-12-22T07:42:01Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 CAN not working Normal mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779096#M29892</link>
      <description>Im usign PTA6&lt;BR /&gt;.pinPortIdx = 6U;&lt;BR /&gt;.mux = PORT_MUX_AS_GPIO;&lt;BR /&gt;driveStrength = PORT_DRIVE_STRENTGTH_NOT_AVAILABLE;&lt;BR /&gt;.inputBuffer = PORT_INPUT_BUFFER_ENABLED;&lt;BR /&gt;.outputBuffer = PORT_OUTPUT_BUFFER_DISABLED;&lt;BR /&gt;.base = IP_SIUL2;&lt;BR /&gt;.safeMode = PORT_SAFE_MODE_DISABLED;&lt;BR /&gt;.inputFilter = PORT_INPUT_FILTER_NOT_AVAILABLE;&lt;BR /&gt;.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED;&lt;BR /&gt;.slewRateCtrlSel = PORT_SLEW_RATE_NOT_AVAILABLE;&lt;BR /&gt;.pullKeep = PORT_PULL_KEEP_DISABLED;&lt;BR /&gt;.invert = PORT_INVERT_DISABLED;&lt;BR /&gt;.adcInterleaves[0U] = MUX_MODE_NOT_AVAILABLE;&lt;BR /&gt;.adcInterleaves[1U] = MUX_MODE_NOT_AVAILABLE;&lt;BR /&gt;.initValue = 2U;&lt;BR /&gt;.inputMuxReg[0U] = 0U;&lt;BR /&gt;.inputMux[0U] = PORT_MUX_ALT4;</description>
      <pubDate>Fri, 22 Dec 2023 07:45:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779096#M29892</guid>
      <dc:creator>rexoplans</dc:creator>
      <dc:date>2023-12-22T07:45:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 CAN not working Normal mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779099#M29894</link>
      <description>&lt;P&gt;&lt;A href="mailto:Hi@rexoplans" target="_blank"&gt;Hi@rexoplans&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;send me your project and i will help you check it next week.&lt;/P&gt;</description>
      <pubDate>Fri, 22 Dec 2023 07:51:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779099#M29894</guid>
      <dc:creator>Senlent</dc:creator>
      <dc:date>2023-12-22T07:51:51Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 CAN not working Normal mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779133#M29895</link>
      <description>&lt;P&gt;Hello rexoplans,i am using s32k312 and configured CAN, are your interrupts configured correctly?, and it should be initialized to work the call_back functions properly, and do you have terminating resistor between the CAN low and CAN high pins?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="saibodhanapu_0-1703233888999.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255641i17FF2ED40CEB81F6/image-size/medium?v=v2&amp;amp;px=400" role="button" title="saibodhanapu_0-1703233888999.png" alt="saibodhanapu_0-1703233888999.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Dec 2023 08:34:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779133#M29895</guid>
      <dc:creator>sai-bodhanapu</dc:creator>
      <dc:date>2023-12-22T08:34:09Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312 CAN not working Normal mode</title>
      <link>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779170#M29897</link>
      <description>"Hello, I believe interrupts are active because my callbacks are functioning properly in loopback mode. There are no termination resistors in between (I knew they weren't necessary at low speeds).</description>
      <pubDate>Fri, 22 Dec 2023 09:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312-CAN-not-working-Normal-mode/m-p/1779170#M29897</guid>
      <dc:creator>rexoplans</dc:creator>
      <dc:date>2023-12-22T09:00:55Z</dc:date>
    </item>
  </channel>
</rss>