<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックRe: SPD demo question</title>
    <link>https://community.nxp.com/t5/S32K/SPD-demo-question/m-p/1778647#M29861</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;yes the highlighted code (Mcu_GetResetReason function) clears the reset flags but the function will also store the reset reason into a global variable for later use. So then when the Mcu_GetResetReason() is called for a second time it will still return the correct reset reason remembered in a global variable of Mcu driver.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Frantisek&lt;/P&gt;</description>
    <pubDate>Thu, 21 Dec 2023 09:48:28 GMT</pubDate>
    <dc:creator>frantisekdobes</dc:creator>
    <dc:date>2023-12-21T09:48:28Z</dc:date>
    <item>
      <title>SPD demo question</title>
      <link>https://community.nxp.com/t5/S32K/SPD-demo-question/m-p/1777090#M29770</link>
      <description>&lt;P&gt;In the main.c file of the demo provided by the&amp;nbsp;&lt;FONT size="4"&gt;S32K3 Safety Peripheral Drivers version 1.0.3&amp;nbsp;&lt;/FONT&gt;&lt;A href="https://nxp.flexnetoperations.com/control/frse/download?element=14273477" target="_blank"&gt;Design : Product Download : Files (flexnetoperations.com)&lt;/A&gt;, I noticed that the first highlighted area clears the reset flags. Doesn't that mean the BIST section will never be executed?&lt;BR /&gt;1. Is this a design flaw or do users need to manually modify certain code?&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pusoy_0-1702979284121.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/255036i77AD0AF60C0BA3DC/image-size/large?v=v2&amp;amp;px=999" role="button" title="Pusoy_0-1702979284121.png" alt="Pusoy_0-1702979284121.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Pusoy_0-1702979284121.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Dec 2023 10:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPD-demo-question/m-p/1777090#M29770</guid>
      <dc:creator>Pusoy</dc:creator>
      <dc:date>2023-12-19T10:00:11Z</dc:date>
    </item>
    <item>
      <title>Re: SPD demo question</title>
      <link>https://community.nxp.com/t5/S32K/SPD-demo-question/m-p/1778647#M29861</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;yes the highlighted code (Mcu_GetResetReason function) clears the reset flags but the function will also store the reset reason into a global variable for later use. So then when the Mcu_GetResetReason() is called for a second time it will still return the correct reset reason remembered in a global variable of Mcu driver.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Frantisek&lt;/P&gt;</description>
      <pubDate>Thu, 21 Dec 2023 09:48:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SPD-demo-question/m-p/1778647#M29861</guid>
      <dc:creator>frantisekdobes</dc:creator>
      <dc:date>2023-12-21T09:48:28Z</dc:date>
    </item>
  </channel>
</rss>