<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 Re: ADC0 reading different channels</title>
    <link>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1777996#M29826</link>
    <description>&lt;P&gt;Thank you&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;, I tried to&amp;nbsp;&lt;SPAN&gt;increase the sample time and&amp;nbsp;decrease the ADC clock, same thing,&lt;BR /&gt;I connected a potentiometer to PTC1 and PTC3 when increasing the resistance on PTC1 without touching&amp;nbsp; the&amp;nbsp;potentiometer on PTC3, and read the values via UART, they both change values.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 20 Dec 2023 13:30:17 GMT</pubDate>
    <dc:creator>DemaQasem</dc:creator>
    <dc:date>2023-12-20T13:30:17Z</dc:date>
    <item>
      <title>ADC0 reading different channels</title>
      <link>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1776889#M29746</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using S32K144 EVB, Design Studio v1.3&lt;/P&gt;&lt;P&gt;I am trying to read 3 sensor's values.&lt;/P&gt;&lt;P&gt;they are connected to (PTC1, PTB2 and PTC3) on ADC0.&lt;BR /&gt;when I connect a potentiometer to PTC1 and read it's value&amp;nbsp;&lt;BR /&gt;all readings (PTC1, PTB2, and PTC3) are affected !&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;the code I used is attached.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 19 Dec 2023 06:55:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1776889#M29746</guid>
      <dc:creator>DemaQasem</dc:creator>
      <dc:date>2023-12-19T06:55:22Z</dc:date>
    </item>
    <item>
      <title>Re: ADC0 reading different channels</title>
      <link>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1777206#M29781</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/215133"&gt;@DemaQasem&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;How effected is the reading?&lt;/P&gt;
&lt;P&gt;The ADC module does not feature pre-sampling to a known value.&lt;/P&gt;
&lt;P&gt;So, the sample-and-hold capacitor keeps the charge from the previous conversion at the start of a new sampling phase.&lt;/P&gt;
&lt;P&gt;If you increase the sample time or decrease the ADC clock, do you get better results?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Tue, 19 Dec 2023 13:25:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1777206#M29781</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-12-19T13:25:21Z</dc:date>
    </item>
    <item>
      <title>Re: ADC0 reading different channels</title>
      <link>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1777996#M29826</link>
      <description>&lt;P&gt;Thank you&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160001"&gt;@danielmartynek&lt;/a&gt;, I tried to&amp;nbsp;&lt;SPAN&gt;increase the sample time and&amp;nbsp;decrease the ADC clock, same thing,&lt;BR /&gt;I connected a potentiometer to PTC1 and PTC3 when increasing the resistance on PTC1 without touching&amp;nbsp; the&amp;nbsp;potentiometer on PTC3, and read the values via UART, they both change values.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Dec 2023 13:30:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1777996#M29826</guid>
      <dc:creator>DemaQasem</dc:creator>
      <dc:date>2023-12-20T13:30:17Z</dc:date>
    </item>
    <item>
      <title>Re: ADC0 reading different channels</title>
      <link>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1778591#M29860</link>
      <description>&lt;P&gt;Can you scope the VREFH and make sure it is stable?&lt;/P&gt;
&lt;P&gt;Have you measured the PTC1 and PTC3 signals using an oscilloscope?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Thu, 21 Dec 2023 09:03:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1778591#M29860</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2023-12-21T09:03:51Z</dc:date>
    </item>
    <item>
      <title>Re: ADC0 reading different channels</title>
      <link>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1779419#M29908</link>
      <description>&lt;P&gt;yes, VREF is stable.&lt;/P&gt;&lt;P&gt;PTC1 &amp;amp; PTC3 voltage is 5V which is the Reference voltage.&lt;/P&gt;</description>
      <pubDate>Sat, 23 Dec 2023 12:12:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1779419#M29908</guid>
      <dc:creator>DemaQasem</dc:creator>
      <dc:date>2023-12-23T12:12:58Z</dc:date>
    </item>
    <item>
      <title>Re: ADC0 reading different channels</title>
      <link>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1781310#M30076</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I checked again ( PTC3 and PTC1) affect each other's readings&lt;BR /&gt;I changed all channels to be (PTB1,PTB2 &amp;amp; PTB3) they worked fine.&lt;/P&gt;&lt;P&gt;but the sensors pins are fixed&lt;BR /&gt;does it help ?&lt;/P&gt;</description>
      <pubDate>Sun, 31 Dec 2023 12:15:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1781310#M30076</guid>
      <dc:creator>DemaQasem</dc:creator>
      <dc:date>2023-12-31T12:15:28Z</dc:date>
    </item>
    <item>
      <title>Re: ADC0 reading different channels</title>
      <link>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1781561#M30105</link>
      <description>&lt;P&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/215133"&gt;@DemaQasem&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Do you inject an current at the pins adjacent to PTC1, PTC3?&lt;/P&gt;
&lt;P&gt;Do you measure the voltage at the PTC1, PTC3, VREF pins during the ADC sampling?&lt;/P&gt;
&lt;P&gt;If the voltage stays stable during the sampling, I don't see any reason to see incorrect results, especially, if you tested it at longer sample time.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jan 2024 08:32:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/ADC0-reading-different-channels/m-p/1781561#M30105</guid>
      <dc:creator>danielmartynek</dc:creator>
      <dc:date>2024-01-02T08:32:57Z</dc:date>
    </item>
  </channel>
</rss>