<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32Kのトピックs32k3 OTA</title>
    <link>https://community.nxp.com/t5/S32K/s32k3-OTA/m-p/1776916#M29748</link>
    <description>&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;After these steps are complete, what is the process of performing an OTA upgrade?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="youxi_0-1702970020777.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/254979i6D49FF6D8EB2B81E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="youxi_0-1702970020777.png" alt="youxi_0-1702970020777.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 19 Dec 2023 07:22:40 GMT</pubDate>
    <dc:creator>youxi</dc:creator>
    <dc:date>2023-12-19T07:22:40Z</dc:date>
    <item>
      <title>s32k3 OTA</title>
      <link>https://community.nxp.com/t5/S32K/s32k3-OTA/m-p/1776916#M29748</link>
      <description>&lt;P&gt;Hi:&lt;/P&gt;&lt;P&gt;After these steps are complete, what is the process of performing an OTA upgrade?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="youxi_0-1702970020777.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/254979i6D49FF6D8EB2B81E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="youxi_0-1702970020777.png" alt="youxi_0-1702970020777.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Dec 2023 07:22:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k3-OTA/m-p/1776916#M29748</guid>
      <dc:creator>youxi</dc:creator>
      <dc:date>2023-12-19T07:22:40Z</dc:date>
    </item>
    <item>
      <title>Re: s32k3 OTA</title>
      <link>https://community.nxp.com/t5/S32K/s32k3-OTA/m-p/1777821#M29812</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Step 2 starts to OTA program the new application App_v2, and step 6 starts to run App_v2. This AN did not program a real new application, just used the copied application(App_v1) as a new application(App_v2) to demonstrate.&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;2. Detect that no valid program exists in the passive partition, &lt;U&gt;copy the same data as the active&lt;/U&gt;&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;&lt;U&gt;partition to the passive partition&lt;/U&gt;, which is Cfg_v1 and App_v1 program code.&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 20 Dec 2023 09:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/s32k3-OTA/m-p/1777821#M29812</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-12-20T09:13:25Z</dc:date>
    </item>
  </channel>
</rss>