<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32KのトピックS32K312</title>
    <link>https://community.nxp.com/t5/S32K/S32K312/m-p/1776169#M29703</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;While looking at the sample code, there is a question. In the example code, the authentication label of an active partition is stored in a passive partition, and the authentication label of the passive partition is stored in an active partition. When implementing secure boot with ab _ awap firmware, do the active block and the passive block applications have to be exactly the same?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 18 Dec 2023 08:05:46 GMT</pubDate>
    <dc:creator>youxi</dc:creator>
    <dc:date>2023-12-18T08:05:46Z</dc:date>
    <item>
      <title>S32K312</title>
      <link>https://community.nxp.com/t5/S32K/S32K312/m-p/1776169#M29703</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;While looking at the sample code, there is a question. In the example code, the authentication label of an active partition is stored in a passive partition, and the authentication label of the passive partition is stored in an active partition. When implementing secure boot with ab _ awap firmware, do the active block and the passive block applications have to be exactly the same?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Dec 2023 08:05:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312/m-p/1776169#M29703</guid>
      <dc:creator>youxi</dc:creator>
      <dc:date>2023-12-18T08:05:46Z</dc:date>
    </item>
    <item>
      <title>Re: S32K312</title>
      <link>https://community.nxp.com/t5/S32K/S32K312/m-p/1777170#M29777</link>
      <description>&lt;P&gt;Duplicate of:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32K/S32K312-SECURE-BOOT/m-p/1777164" target="_blank"&gt;https://community.nxp.com/t5/S32K/S32K312-SECURE-BOOT/m-p/1777164&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 Dec 2023 11:49:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K312/m-p/1777170#M29777</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2023-12-19T11:49:05Z</dc:date>
    </item>
  </channel>
</rss>