<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32K中的主题 S32K116 CAN Receive</title>
    <link>https://community.nxp.com/t5/S32K/S32K116-CAN-Receive/m-p/1775452#M29661</link>
    <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I use CAN in the S32K116.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Sending and receiving works so far.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Now I would like to use the option to store a callback to receive.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;So how do I use CAN_InstallEventCallback?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 15 Dec 2023 08:43:02 GMT</pubDate>
    <dc:creator>tklauke</dc:creator>
    <dc:date>2023-12-15T08:43:02Z</dc:date>
    <item>
      <title>S32K116 CAN Receive</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-CAN-Receive/m-p/1775452#M29661</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I use CAN in the S32K116.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Sending and receiving works so far.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Now I would like to use the option to store a callback to receive.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;So how do I use CAN_InstallEventCallback?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 15 Dec 2023 08:43:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-CAN-Receive/m-p/1775452#M29661</guid>
      <dc:creator>tklauke</dc:creator>
      <dc:date>2023-12-15T08:43:02Z</dc:date>
    </item>
    <item>
      <title>Re: S32K116 CAN Receive</title>
      <link>https://community.nxp.com/t5/S32K/S32K116-CAN-Receive/m-p/1775990#M29685</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Please refer to the examples in&amp;nbsp;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/S32K1xx-SDK-FlexCAN-sample-projects-to-demonstrate-its-basic-and/ta-p/1172891" target="_self"&gt;S32K1xx SDK FlexCAN sample projects to demonstrate its basic and advanced features&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Here you will see how to use&amp;nbsp;&lt;STRONG&gt;CAN_InstallEventCallback &lt;/STRONG&gt;in&amp;nbsp;&lt;EM&gt;S32K144_CAN_PAL_SamplePrj_Basic_TxRx_ID_FiltersConfig_SDKRTM3P0:&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CAN_InstallEventCallback.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/254754i64A734F82B1335C1/image-size/large?v=v2&amp;amp;px=999" role="button" title="CAN_InstallEventCallback.png" alt="CAN_InstallEventCallback.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;CAN_InstallEventCallback.png&lt;/span&gt;&lt;/span&gt;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Robin&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 18 Dec 2023 03:36:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/S32K116-CAN-Receive/m-p/1775990#M29685</guid>
      <dc:creator>Robin_Shen</dc:creator>
      <dc:date>2023-12-18T03:36:02Z</dc:date>
    </item>
  </channel>
</rss>