<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SBC_FS26_example in S32K</title>
    <link>https://community.nxp.com/t5/S32K/SBC-FS26-example/m-p/1775347#M29650</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using SBC_FS26_example and FS26 in my board works in normal mode. However when i try to write something to any registers with Sbc_fs26_WriteRegister(boolean bIsFailSafe, uint8 u8Address, uint16 u16WriteData) function it does not write it. I try to read it with&amp;nbsp;Sbc_fs26_ReadRegister(boolean bIsFailSafe, uint8 u8Address, Sbc_fs26_RxFrameType* pRxData) and i see that i can not write it. What could be the problem?&lt;/P&gt;</description>
    <pubDate>Fri, 15 Dec 2023 06:36:52 GMT</pubDate>
    <dc:creator>Albatros</dc:creator>
    <dc:date>2023-12-15T06:36:52Z</dc:date>
    <item>
      <title>SBC_FS26_example</title>
      <link>https://community.nxp.com/t5/S32K/SBC-FS26-example/m-p/1775347#M29650</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using SBC_FS26_example and FS26 in my board works in normal mode. However when i try to write something to any registers with Sbc_fs26_WriteRegister(boolean bIsFailSafe, uint8 u8Address, uint16 u16WriteData) function it does not write it. I try to read it with&amp;nbsp;Sbc_fs26_ReadRegister(boolean bIsFailSafe, uint8 u8Address, Sbc_fs26_RxFrameType* pRxData) and i see that i can not write it. What could be the problem?&lt;/P&gt;</description>
      <pubDate>Fri, 15 Dec 2023 06:36:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SBC-FS26-example/m-p/1775347#M29650</guid>
      <dc:creator>Albatros</dc:creator>
      <dc:date>2023-12-15T06:36:52Z</dc:date>
    </item>
    <item>
      <title>Re: SBC_FS26_example</title>
      <link>https://community.nxp.com/t5/S32K/SBC-FS26-example/m-p/1776526#M29727</link>
      <description>&lt;P&gt;Hello &lt;SPAN&gt;Albatros&lt;/SPAN&gt;,&lt;/P&gt;
&lt;P&gt;I hope all is great with you. Thank you for using the NXP communities.&lt;/P&gt;
&lt;P&gt;Could you please share more information about the sample code used? I mean, what is the source code?&lt;/P&gt;
&lt;P&gt;What are the registers that you are trying to modify?&lt;/P&gt;
&lt;P&gt;Do you mean that you cannot write it or read it?&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;David&lt;/P&gt;</description>
      <pubDate>Mon, 18 Dec 2023 18:14:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32K/SBC-FS26-example/m-p/1776526#M29727</guid>
      <dc:creator>diazmarin09</dc:creator>
      <dc:date>2023-12-18T18:14:54Z</dc:date>
    </item>
  </channel>
</rss>